Skip to main content
T J
Senior III
May 24, 2018 3:52 AM UTC
Solved

I wish for an upcomming ST event for forum moderators and contributors

Posted on May 24, 2018 at 05:52

We would like to come meet in  France/Europe  maybe in Summer.

We would like to meet all the forum moderators and contributors and possibly book a day or two with the HAL engineers.

ST would hopefully be paying for the flights and accommodation for some of the more prolific contributors.

Then we will be able to work the timeline for the dual display, VR inspired wearable fanless ST-GPU launch.

I will bring the flowers.

    This topic has been closed for replies.
    Andrew Neil
    Andrew NeilBest answer
    Super User
    May 24, 2018 12:34 PM UTC
    Posted on May 24, 2018 at 12:34

    There was plenty to eat and drink ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

    8 replies

    T J
    T JAuthor
    Senior III
    May 24, 2018 5:43 AM UTC
    Posted on May 24, 2018 at 07:43

    The flowers are for

    st.mcu

    ‌

    ELMHIRI.Syrine

    ‌ and

    DAHMEN.IMEN

    ‌ of course...

    Amel NASRI
    ST Technical Moderator
    May 24, 2018 8:42 AM UTC
    Posted on May 24, 2018 at 10:42

    Hi T J,

    Thanks for the flowers and the proposal.

    May you explain more what do you expect from such event: the purpose, what to discuss? what to suggest? who do you suggest to be invited?...

    I add

    Kling.Brian

    ‌ in this discussion.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    T J
    T JAuthor
    Senior III
    May 24, 2018 11:42 AM UTC
    Posted on May 24, 2018 at 11:42

    Its an adventure.

    Free Beer and pizzas for starters.. hehe

    I would like to meet up with

    meyer.frank

    ‌

    Neil.Andrew

    ‌

    garsi.khouloud

    ‌

    Waclawek.Jan

    ‌

    Turvey.Clive

    oliverbeirne

    and the crowd.

    The group could discuss anything that anyone considers at length.

    I am sure everyone has interesting projects to confab over if they want.

    and we can give Clive the inaugural ST-Master Trophy, (we should decide on an Epic title for the trophy.)

    It is interesting to me to see the future in 3D,

    so I thought

    if we are going to make an all new Fluid VR headset, then ST is going to need to know what we need to run it.

    No one person can know everything about a product and foresee short comings.

    Wearable, Fanless Dual 4k 100fps outputs feed into the VR screens.

    Several ARM Cores and at least 16-1024 GPU cores, with 3D Audio Immersion.

    H265 & WebGL are the primary mediums

    Since we are making a new processor family, an optical port would give us TByte transfers with 1 or 2 pins

    Embedded 1GByte Ram or Optical port Ram would be nice, while you are at it.

    Easy enough to run 2x 4K screens over an Optical channel.

    I thought optical would be beneficial in 2 ways.

    Flexible / Wearable and distance is not an issue. (We need upto 3M at most) I guess

    anyhow, my nuts and bolts aren't worked out, hence the need for befuddled conflaberations, pizza and flowers of course.

    Andrew Neil
    Super User
    May 24, 2018 12:10 PM UTC
    Posted on May 24, 2018 at 12:10

    Sounds like you're thinking of something like this: 

    http://blog.antronics.co.uk/2014/06/26/didnt-we-have-a-loverly-time-the-days-we-went-to-paris/

      ?
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Tesla DeLorean
    Guru
    May 24, 2018 11:49 AM UTC
    Posted on May 24, 2018 at 13:49

    As Brian can no doubt recount, I've had this conversation with him where this is exactly not something I want to do.

    http://www.google.com/search?q=busmans+holiday

     
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    T J
    T JAuthor
    Senior III
    May 24, 2018 2:01 PM UTC
    Posted on May 24, 2018 at 14:01

    Neil.Andrew

    said he would do Karaoke,

    He sent me his video...