Skip to main content
IWhit.2
Associate II
July 11, 2022
Question

I want to use the WM8994 on the STM32F769-DISCO for 24 bit acquisition on the Line In connector. Unfortunately the BSP code is fixed at 16 bit. :-(

  • July 11, 2022
  • 0 replies
  • 515 views

Has anyone done the changes necessary to switch up to 24/32 bit acquisition. It seems like its just AIF1_Control[6,5] on the WM8994 but the SAI is a complex beast and I'm not having a lot of luck. Any pointers would be greatly appreciated.

This topic has been closed for replies.