I want to use pwm input capture TIM3 CH1/CH2.
Dear All,
I want to use pwm input capture GPIOA.6 and GPIOA.7 using TIM3 on STM32F407IG(176pin)
Channel 1 and Channel 2 work's fine if I set just one of them.
But channel 1 and channel 2 does not work if I set at the same time.
void TIM3_IRQHandler(void)
{#if 1 if((TIM_GetITStatus(TIM3, TIM_IT_CC1)==SET)) { TIM_ClearITPendingBit(TIM3, TIM_IT_CC1); GetFrequencyCycleCount(NUM1, TIM_GetCapture1(TIM3)); }#endif#if 2
if((TIM_GetITStatus(TIM3, TIM_IT_CC2)==SET)) { TIM_ClearITPendingBit(TIM3, TIM_IT_CC2); GetFrequencyCycleCount(NUM2, TIM_GetCapture2(TIM3)); }#endif}
void TIM3_TimerSet(void)
{ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure; TIM_ICInitTypeDef TIM_ICInitStructure;/* TIM2 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);/* GPIOA clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);/* Enable the TIM3 global Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6|GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOA, &GPIO_InitStructure); //GPIO_PinAFConfig(GPIOA, GPIO_PinSource6|GPIO_PinSource7, GPIO_AF_TIM3); GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_TIM3); GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_TIM3);#if 1
TIM_TimeBaseStructure.TIM_Period = TIMER_PERIOD; TIM_TimeBaseStructure.TIM_Prescaler = 84-1; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);#endif#if 1
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInitStructure.TIM_Channel = TIM_Channel_1; TIM_PWMIConfig(TIM3, &TIM_ICInitStructure);TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;
TIM_PWMIConfig(TIM3, &TIM_ICInitStructure);#endif#if 1 /* Select the TIM3 Input Trigger*/ TIM_SelectInputTrigger(TIM3, TIM_TS_TI1FP1|TIM_TS_TI2FP2);/* Select the slave Mode: Reset Mode */
TIM_SelectSlaveMode(TIM3, TIM_SlaveMode_Reset); TIM_SelectMasterSlaveMode(TIM3,TIM_MasterSlaveMode_Enable);#endif/* TIM enable counter */
TIM_Cmd(TIM3, ENABLE);/* Enable the CC2 Interrupt Request */
TIM_ITConfig(TIM3, TIM_IT_CC1|TIM_IT_CC2, ENABLE);}
#endif