Skip to main content
Ptiwa.11
Visitor II
April 19, 2021
Question

I used SDMMC in STM32H743ZI , SD card mount successful but f_open getting fail, how to solve this issue

static void FS_FileOperations(void) {

FRESULT res; /* FatFs function common result code */

uint32_t byteswritten, bytesread; /* File write/read counts */

uint8_t wtext[] = "This is STM32 working with FatFs uSD + FreeRTOS"; /* File write buffer */

/* Register the file system object to the FatFs module */

if (f_mount(&SDFatFs, (TCHAR const*) SDPath, 0) == FR_OK) {

/* check whether the FS has been already created */

if (isFsCreated == 0) {

if (f_mkfs(SDPath, FM_ANY, 0, workBuffer, sizeof(workBuffer))

!= FR_OK) {

printf("f_mkfs Failed!\r\n");

return;

}

isFsCreated = 1;

}

/* Create and Open a new text file object with write access */

if (f_open(&MyFile, "STM32H7.TXT", FA_CREATE_ALWAYS | FA_WRITE)

== FR_OK) {

/* Write data to the text file */

res = f_write(&MyFile, wtext, sizeof(wtext), (void*) &byteswritten);

if ((byteswritten > 0) && (res == FR_OK)) {

/* Close the open text file */

f_close(&MyFile);

/* Open the text file object with read access */

if (f_open(&MyFile, "STM32H7.TXT", FA_READ) == FR_OK) {

/* Read data from the text file */

res = f_read(&MyFile, rtext, sizeof(rtext),

(void*) &bytesread);

if ((bytesread > 0) && (res == FR_OK)) {

/* Close the open text file */

f_close(&MyFile);

/* Compare read data with the expected data */

if ((bytesread == byteswritten)) {

/* Success of the demo: no error occurrence */

printf(

"Success of the demo: no error occurrence\r\n");

return;

}

}

}

}

}

}

/* Error */

printf("FS_FileOperations\r\n");

}

This topic has been closed for replies.