Skip to main content
Gbasi.1
Associate III
May 4, 2020 1:00 PM UTC
Question

I'm trying to write and read flash

hi guys, im working on stm32l412kb mcu using keil v5 uvision and i ve found it difficult to write and read flash memory. all the explanation online are not relevant for my mcu. that the way i'm trying to confirm my actions, if anyone understand the problem it would be extremely helpful.

{EraseInitStruct.TypeErase=FLASH_TYPEERASE_PAGES;

EraseInitStruct.Banks=FLASH_BANK_1;

EraseInitStruct.Page=255;

EraseInitStruct.NbPages=1;

HAL_FLASH_Unlock();

HAL_FLASHEx_Erase(&EraseInitStruct, &pageError);

HAL_UART_Transmit(&huart1, (uint8_t*)"tried2\n\r", 13,100);

data=*(uint64_t *)0x08000004;

HAL_UART_Transmit(&huart1,(uint8_t*)data, 13,100);

HAL_UART_Transmit(&huart1, (uint8_t*)"\n\rtried3\n\r", 13,100);

HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD,0x08000004,0x01u);

data=*(uint64_t *)0x08000004;

HAL_UART_Transmit(&huart1,(uint8_t*)value, 13,100);

if (value==0x01u)

HAL_UART_Transmit(&huart1, (uint8_t*)"we made it\n\r", 20,100);

else

HAL_UART_Transmit(&huart1, (uint8_t*)"\n\r we are losers\n\r", 20,100);

HAL_FLASH_Lock();

HAL_Delay(100);}

This topic has been closed for replies.

10 replies

TDK
May 4, 2020 1:41 PM UTC

> EraseInitStruct.Page=255;

> EraseInitStruct.NbPages=1;

So you're trying to erase page 255? How many pages of flash does that chip have? Datasheet says 64.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Gbasi.1
Gbasi.1Author
Associate III
May 4, 2020 1:59 PM UTC

Thanks so much for the help, you're right. But even though I changed it, the code still doesn't work. The values ​​are not equal to each other:

EraseInitStruct.TypeErase=FLASH_TYPEERASE_PAGES;

EraseInitStruct.Banks=FLASH_BANK_1;

EraseInitStruct.Page=63;

EraseInitStruct.NbPages=1;

HAL_FLASH_Unlock();

HAL_FLASHEx_Erase(&EraseInitStruct, &pageError);

HAL_UART_Transmit(&huart1, (uint8_t*)"tried2\n\r", 13,100);

data=*(uint64_t *)0x08000004;

HAL_UART_Transmit(&huart1,(uint8_t*)data, 13,100);

HAL_UART_Transmit(&huart1, (uint8_t*)"\n\rtried3\n\r", 13,100);

HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD,0x08000004,0x01u);

data=*(uint64_t *)0x08000004;

HAL_UART_Transmit(&huart1,(uint8_t*)value, 13,100);

if (value==0x01u)

HAL_UART_Transmit(&huart1, (uint8_t*)"we made it\n\r", 20,100);

else

HAL_UART_Transmit(&huart1, (uint8_t*)"\n\r we are losers\n\r", 20,100);

HAL_FLASH_Lock();

HAL_Delay(100);}

berendi
Principal
May 4, 2020 2:30 PM UTC

Read chapter 3 of the reference manual, with close attention to the section titled Flash main memory programming sequences.

data=*(uint64_t *)0x08000004;

Data should be aligned to doubleword addresses, i.e. ones that are evenly divisible by 8. The address above is not.

Moreover, it does not point to the address range that have been erased, but attempting to overwrite the reset address of the program itself. See Flash memory organization at the top of chapter 3.

Gbasi.1
Gbasi.1Author
Associate III
May 4, 2020 2:35 PM UTC

thanx berendi, can you please send me a link to that menual, just to be sure im reading the correct file.

and if u can suggest a different way to do that it would be great!

Tesla DeLorean
Guru
May 4, 2020 2:57 PM UTC

https://www.st.com/en/microcontrollers-microprocessors/stm32l412kb.html

Data Sheet

https://www.st.com/resource/en/datasheet/stm32l412kb.pdf

Reference Manual

https://www.st.com/resource/en/reference_manual/dm00151940-stm32l41xxx42xxx43xxx44xxx45xxx46xxx-advanced-armbased-32bit-mcus-stmicroelectronics.pdf

Use the address of the page/sector you are erasing, and don't use the front of FLASH where your executing code is situated.

Find a better way to send 64-bit values, perhaps sprintf() into ASCII, and then send. Write a subroutine to wrap the UART Transmit so it computes the length of the string, rather than you putting in constants.

char asciidata[32];

uint64_t value =*(uint64_t *)0x08000004;

HAL_UART_Transmit(&huart1,(uint8_t*)asciidata, sprintf(asciidata,"%lx\n", value),250); // don't recall 64-bit format, but sprintf() returns length

One the readback use the value, not data variable.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Piranha
Principal III
May 6, 2020 10:23 AM UTC
data=*(uint64_t *)0x08000004;

This code can be written only by someone, who hasn't read anything at all! The reference manual section 3.3.7 describes a different programming procedure and HAL_FLASH_Program() code also shows how to do it.

Gbasi.1
Gbasi.1Author
Associate III
May 6, 2020 10:30 AM UTC

hi, im new in this.

i tried to read it but apparently didnt understood too much.

if you dont mind to enplane a little bit more.

all im trying to do is to write a number to 0x08000004, then to read it for confirmation.

what should i do?

berendi
Principal
May 6, 2020 10:57 AM UTC

Then go back to the basics. You won't get too far without it.

How is computer memory organized in general, and specifically on the Cortex-M platform? What is a byte, halfword, word, doubleword? How are they stored in memory, how can they be addressed? What is alignment, what is the difference between aligned an unaligned addresses and accesses?

How does flash memory work? What is the basic difference from the user's point of view between eeprom and flash type memory?

How is a program stored in memory in general, and specifically on the Cortex-M platform? Where and how does program execution start, what happens after reset?

Gbasi.1
Gbasi.1Author
Associate III
May 6, 2020 2:08 PM UTC

ive been reading those topics since i started work on the project. i am not exactly understand the last 3 topics you mentioned so thats the point where i stoped. if you can direct me specifically with stm32l412 it would be great couse all the The things I find are associated with other processors.

If you can specifically point out the problem with my code it would be best.

berendi
Principal
May 6, 2020 2:34 PM UTC

I have already pointed out the problems with your code.

Data should be aligned to doubleword addresses, i.e. ones that are evenly divisible by 8. The address above is not.

Moreover, it does not point to the address range that have been erased, but attempting to overwrite the reset address of the program itself. 

There is nothing specific to the stm32l412 in it.

Read chapter 3 of the reference manual. I can't read it for you. If there are terms that you don't understand, like alignment, look them up.