Skip to main content
mymy49
Associate
June 25, 2015
Question

I'm Trying to Enable SDRAM without STM32 Library. But Not works.

  • June 25, 2015
  • 4 replies
  • 1180 views
Posted on June 25, 2015 at 07:36

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    June 25, 2015
    Posted on June 25, 2015 at 15:07

    Suggest you take the SPL code that does the configuration properly and bisect against yours until you understand which piece is ''not working''.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mymy49
    mymy49Author
    Associate
    June 25, 2015
    Posted on June 25, 2015 at 17:11

    dear clive1.

    thank you your reply.

    I was Trying to compare with STM32 Library.

    I think, This source code is almost same configuration process with STM32 Library.

    I am confused.

    mymy49
    mymy49Author
    Associate
    June 25, 2015
    Posted on June 25, 2015 at 17:13

    I was Attached all source code Files now.

    Mark Edwards
    Associate III
    June 25, 2015
    Posted on June 25, 2015 at 20:48

    That looks very complicated. This works for STM32F429 Discovery board.

    void SDRAM_Init (void) {
    uint32_t temp32;
    /* GPIO configuration for FMC SDRAM bank */
    /*
    +-------------------+--------------------+--------------------+--------------------+
    + SDRAM pins assignment +
    +-------------------+--------------------+--------------------+--------------------+
    | PD0 <-> FMC_D2 | PE0 <-> FMC_NBL0 | PF0 <-> FMC_A0 | PG0 <-> FMC_A10 |
    | PD1 <-> FMC_D3 | PE1 <-> FMC_NBL1 | PF1 <-> FMC_A1 | PG1 <-> FMC_A11 |
    | PD8 <-> FMC_D13 | PE7 <-> FMC_D4 | PF2 <-> FMC_A2 | PG2 <-> FMC_A12 | <<<
    NEW
    for 64MB
    | PD9 <-> FMC_D14 | PE8 <-> FMC_D5 | PF3 <-> FMC_A3 | PG8 <-> FMC_SDCLK |
    | PD10 <-> FMC_D15 | PE9 <-> FMC_D6 | PF4 <-> FMC_A4 | PG15 <-> FMC_NCAS | 
    | PD14 <-> FMC_D0 | PE10 <-> FMC_D7 | PF5 <-> FMC_A5 |--------------------+ 
    | PD15 <-> FMC_D1 | PE11 <-> FMC_D8 | PF11 <-> FMC_NRAS | 
    +-------------------| PE12 <-> FMC_D9 | PF12 <-> FMC_A6 | 
    | PE13 <-> FMC_D10 | PF13 <-> FMC_A7 | 
    | PE14 <-> FMC_D11 | PF14 <-> FMC_A8 |
    | PE15 <-> FMC_D12 | PF15 <-> FMC_A9 |
    +-------------------+--------------------+--------------------+
    | PB5 <-> FMC_SDCKE1| 
    | PB6 <-> FMC_SDNE1 | 
    | PC0 <-> FMC_SDNWE |
    +-------------------+ 
    */
    // GPIOB Configuration - PB.6&5
    GPIOB->MODER = GPIOB->MODER | 0x2800; // Alt Fn
    GPIOB->OSPEEDR = GPIOB->OSPEEDR | 0x2800; // 50MHz
    GPIOB->AFR[0] = GPIOB->AFR[0] | 0x0CC00000; // SDRAM
    // GPIOC Configuration - PC.0
    GPIOC->MODER = GPIOC->MODER | 0x2; // Alt Fn
    GPIOC->OSPEEDR = GPIOC->OSPEEDR | 0x2; // 50MHz
    GPIOC->AFR[0] = GPIOC->AFR[0] | 0xC; // SDRAM
    // GPIOD Configuration - PD.15,14,10,9,8,1,0
    GPIOD->MODER = GPIOD->MODER | 0xA02A000A; // Alt Fn
    GPIOD->OSPEEDR = GPIOD->OSPEEDR | 0xA02A000A; // 50MHz
    GPIOD->AFR[0] = GPIOD->AFR[0] | 0xCC; // SDRAM AFRL
    GPIOD->AFR[1] = GPIOD->AFR[1] | 0xCC000CCC; // SDRAM AFRH
    // GPIOE Configuration - PE.15,14,13,12,11,10,9,8,7,1,0
    GPIOE->MODER = GPIOE->MODER | 0xAAAA800A; // Alt Fn
    GPIOE->OSPEEDR = GPIOE->OSPEEDR | 0xAAAA800A; // 50MHz
    GPIOE->AFR[0] = GPIOE->AFR[0] | 0xC00000CC; // SDRAM AFRL
    GPIOE->AFR[1] = GPIOE->AFR[1] | 0xCCCCCCCC; // SDRAM AFRH
    // GPIOF Configuration - PE.15,14,13,12,11,5,4,3,2,1,0
    GPIOF->MODER = GPIOF->MODER | 0xAA800AAA; // Alt Fn
    GPIOF->OSPEEDR = GPIOF->OSPEEDR | 0xAA800AAA; // 50MHz
    GPIOF->AFR[0] = GPIOF->AFR[0] | 0xCCCCCC; // SDRAM AFRL
    GPIOF->AFR[1] = GPIOF->AFR[1] | 0xCCCCC000; // SDRAM AFRH
    // >>>OLD PRE A12 - 64MB SDRAM
    // // GPIOG Configuration - PG.15,8,5,4,1,0
    // GPIOG->MODER = GPIOG->MODER | 0x80020A0A; // Alt Fn
    // GPIOG->OSPEEDR = GPIOG->OSPEEDR | 0x80020A2A; // 50MHz
    // GPIOG->AFR[0] = GPIOG->AFR[0] | 0xCC00CC; // SDRAM AFRL
    // GPIOG->AFR[1] = GPIOG->AFR[1] | 0xC000000C; // SDRAM AFRH
    // GPIOG Configuration - PG.15,8,5,4,2,1,0 >>>NEW A12<<<
    GPIOG-
    >MODER = GPIOG->MODER | 0x80020A2A; // Alt Fn
    GPIOG->OSPEEDR = GPIOG->OSPEEDR | 0x80020A2A; // 50MHz
    GPIOG->AFR[0] = GPIOG->AFR[0] | 0xCC0CCC; // SDRAM AFRL
    GPIOG->AFR[1] = GPIOG->AFR[1] | 0xC000000C; // SDRAM AFRH
    // Enable Peripheral Clock
    RCC->AHB3ENR = RCC->AHB3ENR | 0x1; // Enable FMC
    // FMC SDRAM bank initialization
    FMC_Bank5_6->SDCR[0] = 0x2800;
    FMC_Bank5_6->SDCR[1] = 0x1D4; //>>>Old 4MB SDRAM<<<
    // 
    FMC_Bank5_6-
    >SDCR[1] = 0x1DB; // 64MB Device
    FMC_Bank5_6->SDTR[0] = 0x106000;
    FMC_Bank5_6->SDTR[1] = 0x10361;
    // FMC SDRAM device initialisation sequence 
    // Configure a clock configuration enable command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0x9; // Send Command
    //need 100ms delay
    for (temp32 = 0x00; temp32 < 
    0xD0000
    ; temp32++)
    {
    temp32
    = temp32;
    }
    // Configure a PALL (precharge all) command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0xA; // Send Command
    // Configure a Auto-Refresh command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0x6B; // Send First Command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0x6B; // Send Second Command
    // Configure a load Mode register command
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    FMC_Bank5_6->SDCMR = 0x4620C; // Send Command
    // Set the refresh rate counter
    FMC_Bank5_6->SDRTR = 0x556;
    while (FMC_Bank5_6->SDSR & 0x20) { // Controller not ready for new request
    };
    /* Disable write protection */
    temp32 = FMC_Bank5_6->SDCR[0]; 
    FMC_Bank5_6->SDCR[0] = (temp32 & 0xFFFFFDFF);
    }