Skip to main content
temo castro
Associate
Sep 25, 2017 10:07 PM UTC
Solved

I have win7, just installed the Unicleo-Gui to Nucleo-F401RE

Posted on September 26, 2017 at 00:07

My problem is Unicleo cant see any port, why?

STM32 ST-LINK Utility works perfectly, I can download/upgrade firmware but no success to Unicleo-Gui

Do I need to install something else?

    This topic has been closed for replies.
    temo castro
    temo castroBest answer
    Associate
    Sep 27, 2017 1:54 PM UTC
    Posted on September 27, 2017 at 15:54

    Is working now, what I did it to load the hex file for

    X-NUCLEO-IKS01A2 Acceleration calibration and after that it communicates, it seems the out-of-the-shelve F401RE comes with a program that doesn't communicate with Unicleo

    2 replies

    temo castro
    temo castroAuthorBest answer
    Associate
    Sep 27, 2017 1:54 PM UTC
    Posted on September 27, 2017 at 15:54

    Is working now, what I did it to load the hex file for

    X-NUCLEO-IKS01A2 Acceleration calibration and after that it communicates, it seems the out-of-the-shelve F401RE comes with a program that doesn't communicate with Unicleo

    hushel
    Associate II
    Jan 6, 2018 9:11 PM UTC
    Posted on January 06, 2018 at 21:11

    I see this same problem, and your solution fixed it for me. They should update the docs to reflect this. Thanks!