Skip to main content
MCade
Visitor II
September 18, 2018
Question

I have tried changing the GPIO output speed and then toggled the output and monitored it on a scope. There is a slight increase in rise time with the speed set to 50MHz, but otherwise very little difference. Why is this?

  • September 18, 2018
  • 2 replies
  • 614 views

..

    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    September 18, 2018

    Which mcu?

    Try to load the output with significant capacitance, tens of pF. Also, switch on the compensation cell, if your mcu has one.

    JW

    Bob S
    Super User
    September 18, 2018

    What kind of load to you have on that pin? Is it connected to anything? Depending on the load you may not see any (or much) difference. For example, a pin with no connection or one driving a high-impedence/low capacitance load won't show much difference. A pin driving a low impedence and/or high capacitance load will show a big difference.