Skip to main content
kb24
Senior
March 7, 2020
Question

I have stm32f407vg discovery board. I could program my board successfully before but now my pc can't recognize debugger. What should I do to fix it?

..

    This topic has been closed for replies.

    8 replies

    TDK
    March 8, 2020

    Undo what you did to make it stop working.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    kb24
    kb24Author
    Senior
    March 8, 2020

    I dont know what caused this, actually I have a guess. I touched the debugger and led turned off. So static might caused this. Any suggestion?

    TDK
    March 8, 2020

    ESD can definitely kill things. If it's a ST board, and the computer can't recognize the debugger after a reset, I would guess it's dead. Although that would be uncommon. Does it show up as connected in the device manager? Does the board have the correct voltage level? Not sure if the LED is tied directly to power or not, but you could check that in the schematic to help diagnose.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    kb24
    kb24Author
    Senior
    March 8, 2020

    I have discovery board.


    _legacyfs_online_stmicro_images_0693W0000000ASYQA2.pngDevice manager says unknown usb device (device identifier operation failed). On 5 V pin I measured 4.78 V and 3V pin 2.99 V.

    Led that turned off is COM led.

    TDK
    March 8, 2020
    If COM is neither red nor green and your chip has power, then likely your onboard ST-Link chip is fried. The actual MCU might be fine.
    "If you feel a post has answered your question, please click ""Accept as Solution""."
    kb24
    kb24Author
    Senior
    March 8, 2020

    So is there any way to fix it or it is dead?

    TDK
    March 8, 2020
    Assuming that's the problem, the ST-Link chip is dead.
    You can still connect to the MCU chip if you have another ST-Link available. You need the NRST, SWDIO and SWCLK lines connected.
    Probably easier to buy a new board though.
    "If you feel a post has answered your question, please click ""Accept as Solution""."
    kb24
    kb24Author
    Senior
    March 8, 2020

    Okay. Thanks.