Skip to main content
HAli.2
Associate
February 9, 2022
Question

i have STM32F103C8T6 suddenly the pins of the MCU is not working. Are the pins fried ? The 3.3v or 5v pins does not work when I connect a LED using 1k res. But when i try to run the Blinky app in eclipse and choose the internal LED PC13 to blink it w

  • February 9, 2022
  • 6 replies
  • 1702 views

..

This topic has been closed for replies.

6 replies

TDK
February 9, 2022

If you can connect to the chip, it's probably fine, especially as PC13 works. Verify LED polarity. What pin are you trying to use? Verify the hardware connection is there.

Always a possibility that a pin is damaged, but they don't damage themselves. Had to be an event that caused it.

"If you feel a post has answered your question, please click ""Accept as Solution""."
HAli.2
HAli.2Author
Associate
February 10, 2022

The LED is working well and i already made sure of that. But with alot of testing i figured out that the problem is in the GND pins of the MCU somehow.

Javier1
Principal
February 10, 2022

What if the LED yure trying to connect is broken or with the wrong polarity?

hit me up in https://www.linkedin.com/in/javiermuñoz/
HAli.2
HAli.2Author
Associate
February 10, 2022

Well, I have already made sure of that. I connected an external 3.3v and it works well

Javier1
Principal
February 10, 2022

if your internal PC13 (green if youre using a bluepill) is working and your external LED is not , there is a hardware/wiring problem.

Could you show us your setup?(pìctures)

hit me up in https://www.linkedin.com/in/javiermuñoz/