Skip to main content
chuan
Visitor II
January 22, 2023
Question

I had some issues with USART3 with nucleo-H723. The board's UART3 is connected to st-linkV3,When I using USART3 to send data in keil, it works fine,but when I use Clion is, the PC serial port shows packet loss, and I want to know what is the reason a

  • January 22, 2023
  • 1 reply
  • 680 views

..

This topic has been closed for replies.

1 reply

S.Ma
Principal
January 22, 2023

Well run a test sending continuously a text and user teraterm type app to check if any missing/skipped data. If not, the issue is probaby in CLion side, which you should send a post to the related community site.