Skip to main content
hjuns
Associate II
Jul 23, 2021 8:17 AM UTC
Solved

I'd like to use the same firmware for different types of MCU.

Hello everyone,

​

​I faced a shortage of MCU materials.

So I found an MCU that uses the same pin map.

I would like to change STM32F767IIT to STM32F767IGT.

​

  1. Please let me know if the change is okay.
  2. Clock does not work when using STM32F767IGT.

If bootloader is used, systick will not work; if disabled, systick will work.

( bootloader is STM32F767IIT firmware).

I need help.

Please answer me.

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
Jul 23, 2021 8:28 AM UTC

Hello,

F767 to F767 is fine, and you shouldn't have differences between both.

>> Clock does not work when using STM32F767IGT.

Your Systick issue is probably not related to the change of the flash size.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

3 replies

Mike_ST
Mike_STBest answer
ST Technical Moderator
Jul 23, 2021 8:28 AM UTC

Hello,

F767 to F767 is fine, and you shouldn't have differences between both.

>> Clock does not work when using STM32F767IGT.

Your Systick issue is probably not related to the change of the flash size.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
hjuns
hjunsAuthor
Associate II
Jul 23, 2021 8:59 AM UTC

Thank you for your answer. :grinning_face:

​

You mean can I use the firmware made with stm32f767ii for 767IG?

Mike_ST
ST Technical Moderator
Jul 23, 2021 9:12 AM UTC

It is always better to adapt/recompile your firmware for your specific target.

But as long as your firmware fits in 1MB flash and don't make use of flash blocks after the 1MBytes limit,

I don't see any reason why it won't work.

Anyways you know better your own design, do the appropriate checks.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.