Skip to main content
Visitor II
October 11, 2024
Question

I can't read TS_CAL1 and TS_CAL2 values from STM32L152RBT6 Flash Memory

I am working with the internal temperature sensor and the VREFINT channel on the STM32L1 series. When I attempt to read the TS_CAL1 and TS_CAL2 calibration values from the flash memory, as specified in the reference manual, I either receive 0 or find it impossible to read the values. Additionally, when I access the flash memory, I find no values stored at the specified addresses. Could this be a hardware issue with my MCU, or is there something else I should be considering?

NADN20_0-1728650904835.png

I am currently working with this formula from the reference manual for the STM32L152RBX, which states that calibration values can be found in the flash memory. However, when I access these memory addresses, I do not find any values. I would like to know if using these calibrated values is essential for my calculations or if I can perform my own calculations without this data

NADN20_1-1728650934946.png

I have been using my own calculations to determine the temperature, including calculating TS_CAL1 and TS_CAL2 values. However, I would like to read the TS_CAL1 and TS_CAL2 values directly from the flash memory for better accuracy.

NADN20_2-1728650965732.png

NADN20_3-1728651004880.png

When I try to read the VREFINT_CAL values from the flash memory, as recommended in the reference manual, the memory locations return 0.I would appreciate any help or advice on this matter.

 

This topic has been closed for replies.

1 reply

Visitor II
October 11, 2024

Hello ,
I think you're pointing to the wrong adress 0x1FFF0078 instead of pointing to 0x1FFF007B .