Question
I am working with STM32G4 NUCLEO and STM32CubeIDE. Created a project to use FDCAN2 (classic mode) to evaluete CAN comm in polling mode. On FDCAN2 CAN messages are only received when I additionally activate FDCAN1.
FDCAN1 has a basic parameter 'Clock Divider' set to 'Divide kernal clock by 1'. FDCAN2 does not have this parameter. In library function HAL_FDCAN_INIT(...) there is a statement:
/* Check FDCAN instance */
if (hfdcan->Instance == FDCAN1)
{
/* Configure Clock divider */
FDCAN_CONFIG->CKDIV = hfdcan->Init.ClockDivider;
}
Without FDCAN1 activated the clock devider is not configured.
How can I use FDCAN2 without FDCAN1 ?