Skip to main content
Sbadi.1
Associate
January 21, 2020
Question

I am using CAN Communication between two STM32F429ZI Microcontroller i am not able to receive the Interrupt callback HAL_CAN_RxFifo0MsgPendingCallback() after receiving the Transmitted Data.

  • January 21, 2020
  • 1 reply
  • 544 views

I am using this Flow for Transmitting Data and Receiving If Anything I am Missing From Flow of Execution wise i am not getting Receiver Callback.

 filterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;

  filterConfig.FilterIdHigh = 0;

  filterConfig.FilterIdLow = 0;

  filterConfig.FilterMaskIdHigh = 0x0000;

  filterConfig.FilterMaskIdLow = 0x0000;

  filterConfig.FilterScale = CAN_FILTERSCALE_32BIT;

  filterConfig.FilterActivation = CAN_FILTER_ENABLE;

  filterConfig.FilterMode = CAN_FILTERMODE_IDMASK;

  filterConfig.FilterBank = 0;

  filterConfig.SlaveStartFilterBank = 0;

  /*##-2- Configure the CAN Filter ###########################################*/

  if( HAL_CAN_ConfigFilter(&hcan1, &filterConfig) != HAL_OK )

  {

  strcpy((char *)pData,"failCFG");

  HAL_UART_Transmit( &huart1,pData, 10, 10 );

  }

  /*##-3- Start the CAN peripheral ###########################################*/

  if (HAL_CAN_Start(&hcan1) != HAL_OK)

  {

  /* Start Error */

  Error_Handler();

  }

  /*##-4- Activate CAN RX notification #######################################*/

  if (HAL_CAN_ActivateNotification(&hcan1,CAN_IT_RX_FIFO0_MSG_PENDING ) != HAL_OK)

  {

  /* Notification Error */

  Error_Handler();

  }

void CAN1_Tx( void )

{

CAN_TxHeaderTypeDef TxHeader;

uint32_t TxMailBox;

TxHeader.DLC = 2;

TxHeader.StdId = CAN_TRANSMIT_ID;

  TxHeader.IDE = CAN_ID_STD;

  TxHeader.RTR = CAN_RTR_DATA;

  TxHeader.ExtId = 0x01;

  TxHeader.TransmitGlobalTime = DISABLE;

  aTxData[0] = ubKeyNumber;

  aTxData[1] = 0xAD;

  if( ubKeyNumber == 0x2 )

  {

   ubKeyNumber = 0x0;

  }

  if( HAL_OK != HAL_CAN_AddTxMessage( &hcan1, &TxHeader, aTxData, &TxMailBox ) )

{

strcpy((char *)pData,"failed\r\n");

HAL_UART_Transmit( &huart1,pData, 10, 10 );

}

//while( HAL_CAN_IsTxMessagePending(&hcan1, TxMailBox ) );

  while(HAL_CAN_GetTxMailboxesFreeLevel(&hcan1) != 3) {}

strcpy((char *)pData,"msgSucees");

HAL_UART_Transmit( &huart1,pData, 10, 10 );

HAL_Delay(200);

LED_Switch(++ubKeyNumber);

}

If anything I am Missing For Enabling Rx Interrupt Let me know

This topic has been closed for replies.

1 reply

Sbadi.1
Sbadi.1Author
Associate
February 6, 2020

I got The RX Interrupt Callback. because of hardware issue on Transceiver so after fixing that i got the message what i transmitted.