Question
I am trying to setup UART on an STM32L072CZTX. I am using interrupt mode and the interrupt seems to be firing due to a pause in main loop execution but nothing inside the interrupt seems to be occurring
I am trying to setup UART on an STM32L072CZTX. In the ioc file I have setup the pins, RX is set to AF4 pullup, and TX is AF4 nopull. The interrupt is set to 0 and enabled. I have redefined the RxCpltCallback in the main and have events occur in there that work when run from main. I can see a pause in main execution (a simple blinking light) but nothing inside the interrupt seems to be happening, flags being set or a different LED blinking.