Skip to main content
swald.18
Visitor II
October 25, 2018
Question

I am trying to interface TM12864H6CCGWA-1 via SPI on nucleo-L073RZ .I am unable to print anything on display. I have checked all connections , all pins are connected correctly but Its not working. Please help me.

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32l0xx_hal.h"
 
/* USER CODE BEGIN Includes */
/*LCD RST */
# define LCD_RST1 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_SET);
# define LCD_RST0 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);
 
/*LCD CS */
# define LCD_CS1 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_2, GPIO_PIN_SET);
# define LCD_CS0 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_2, GPIO_PIN_RESET);
 
/* LCD RS */
# define LCD_RS1 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_1, GPIO_PIN_SET);//A0
# define LCD_RS0 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_1, GPIO_PIN_RESET);
 
 
/* LCD SCK */
# define LCD_SCK1 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);//SCK
# define LCD_SCK0 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
 
/* LCD MOSI */
# define LCD_MOSI1 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, GPIO_PIN_SET);//SDA
# define LCD_MOSI0 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, GPIO_PIN_RESET);
 
/* USER CODE END Includes */
 
/* Private variables ---------------------------------------------------------*/
SPI_HandleTypeDef hspi1;
 
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
uint8_t aTxBuffer[2];
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI1_Init(void);
 
 
/**
 * @brief The application entry point.
 *
 * @retval None
 */
void lcd_send_cmd(unsigned char cmd)
{
 aTxBuffer[0]= (cmd&0x0f)|0x04;
 aTxBuffer[1]= (cmd&0x0f);
 LCD_RS0;
 LCD_CS0;
 LCD_SCK0;
for(int i=0;i<8;i++){
 LCD_SCK0;
	 if( cmd & 0x0f){
		 LCD_MOSI1;}
	 else
		 {LCD_MOSI0;}
		 LCD_SCK1;
		 HAL_Delay(100);
		// LCD_SCK0;
		 cmd<<=1;
	 }
 HAL_SPI_Transmit(&hspi1,&cmd,2,100);
 while (HAL_SPI_GetState(&hspi1)!= HAL_SPI_STATE_READY);
 LCD_MOSI0;
 LCD_CS1;
}
 
void lcd_send_data(unsigned char data)
{
 aTxBuffer[0]= (data&0x0f)|0x04;
 aTxBuffer[1]= (data&0x0f);
	 LCD_RS1;
	 LCD_CS0;
	 LCD_SCK0;
for(int i=0;i<8;i++)
	{
 LCD_SCK0;
		 HAL_Delay(100);
	 if (data & 0x0f)
	{LCD_MOSI1;}
 else {LCD_MOSI0;}
	 LCD_SCK1;
		HAL_Delay(100);
 
		data<<=1;
	 }
	 HAL_SPI_Transmit(&hspi1,&data,2,100);
	 while (HAL_SPI_GetState(&hspi1)!= HAL_SPI_STATE_READY);
	 LCD_MOSI0;
 LCD_CS1;
 
}
 
void set_rr(char rr)	//0<=rr<=7
{
 LCD_RS0;
	lcd_send_data((0x20)|((rr)&(0x07)));
}
void set_ev(char ev)	//0<=ev<=63
{
	LCD_RS0;
	lcd_send_data(0x81);
	lcd_send_data(((0x3F)&(ev)));
}
void power_control(char dat)	//0<=dat<=7
//dat=1: Built-in Follower ON
//dat=2: Built-in Regulator ON
//dat=4: Built-in Booster ON
{
	LCD_RS0;
	dat=((dat)&(0x07));
	lcd_send_data(((0x28)|(dat)));
}
 
// update lcd
 
void copy_to_lcd(void)
{
 for (int page = 0; page < 8; page++) {
 lcd_send_cmd(0x00); // set column low nibble 0
 lcd_send_cmd(0x10); // set column hi nibble 0
 lcd_send_cmd(0xB0|page); // set page address 0
 LCD_RS1;
 
 for(int i=page*128; i<(page*128+128); i++) {
 lcd_send_data(aTxBuffer[i]);
 }
 }
}
void lcd_Init(void)
{
 // LCD_RS0;
	//LCD_CS1;
	LCD_RST0;
	HAL_Delay(100);
	LCD_RST1;
 
 lcd_send_cmd (0xE2);//Sw RESWT
	 HAL_Delay(100);
 
 lcd_send_cmd (0xA2);//LCD bias
	 HAL_Delay(100);
 
 lcd_send_cmd (0xAF);//display on
	 HAL_Delay(100);
 
 lcd_send_cmd (0xA0);//Segment direction
	 HAL_Delay(100);
 
 lcd_send_cmd (0xC8);//common direction
	 HAL_Delay(100);
 
 set_rr(0x04);//Regulation resistor select
	 HAL_Delay(100);
 
 set_ev(0x1F);;//EV select
	 HAL_Delay(100);
 
	 power_control(0x07);	//ALL Power Control ON
	 HAL_Delay(100);
 
 
 lcd_send_cmd (0x40);//Initial display line 40
	 HAL_Delay(100);
 
 lcd_send_cmd (0xB0);//set page address
	 HAL_Delay(100);
 
 lcd_send_cmd (0x10);//set colmn address MSB
	 HAL_Delay(100);
 
 lcd_send_cmd (0x00);//set column address LSB
	 HAL_Delay(100);
 
 lcd_send_cmd (0xAF);//display on
	 HAL_Delay(100);
	 lcd_send_cmd (0xA4);//normal display , all pixels on
	 HAL_Delay(100);
 
 copy_to_lcd();
 
}
 
 
void lcd_send_string (char *str)
 
{
 while (*str) lcd_send_data (*str++);
 
}
 
 
void lcd_set_pixel(int x, int y, int color)
{
 int page,col;
 int row_in_page;
 
 page = y / 8;
 
 /* Selecting Page */
 lcd_send_cmd(0xB0 | page);
 
 /* Selecting Column */
 col = ((x & 0xf0) >> 4) | 0x10;
 lcd_send_cmd(0x10|col);
 lcd_send_cmd(x & 0xf0);
 
 /* Pixel location */
 row_in_page = y % 8;
 
#ifdef CONFIG_LARGE_MEMORY
 if (color)
 gfx_buf[page][col] |= 1 << row_in_page;
 else
 gfx_buf[page][col] &= ~(1 << row_in_page);
 
 glcd_write_data(gfx_buf[page][col]);
#else
 if (color)
 lcd_send_data(1 << row_in_page);
#endif
 
}
/**
 * @brief The application entry point.
 *
 * @retval None
 */
int main(void)
{
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
// printf("Hello");
 HAL_Init();
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_SPI1_Init();
 LCD_RST0;
	HAL_Delay(100);
	LCD_RST1;
 lcd_Init();
	lcd_send_cmd(0xB0);
	lcd_send_cmd(0x00);
	lcd_send_data(0xFF);
	lcd_send_string("Its working");
	for (int i = 0; i < 128; i++)
 { for (int j = 0; j < 64; j++)
 {lcd_set_pixel(i, j, 1);
	 }
 return 0;}
 
}
 

    This topic has been closed for replies.