Skip to main content
DBara.3
Associate
March 20, 2022
Solved

I am struggling trying to locate a library header in a specific address. Header has a limited size Error is: ld.exe: DiscoL496_07.elf section `CLIENT_HDR' will not fit in region `CLIENT_ROM' ld.exe: region `CLIENT_ROM' overflowed by 269730352 bytes

The structure of the code is:

  • A library called "clientManiobra.a" to be placed in "CLIENT_ROM" memory region. Library requires to place a struct constant in the very first position in "CLIENT_ROM" memory
  • The above library to be linked with main application.

Application's memory map ("memory_map.ld"):

/* Common memory definition */
MEMORY
{
	SHARED_RAM (xrw)	: ORIGIN = 0x20000000,		LENGTH = 256
	RAM (xrw)	: ORIGIN = 0x20000100, 		LENGTH = 320K - LENGTH(SHARED_RAM)
	BOOT_FLASH (rx)		: ORIGIN = 0x08000000,		LENGTH = 32K
	SLOT1_ROM (rx) 	: ORIGIN = 0x08008000, 	LENGTH = 360k
	SLOT2_ROM (rx)		: ORIGIN = 0x08062000,		LENGTH = 360k
	CLIENT_ROM (rx)		: ORIGIN = 0x080BC000,		LENGTH = 240k
	SHARED_CFG (rx)		: ORIGIN = 0x080F8000,		LENGTH = 32k
}
 
/* SHARED_RAM is memory to pass messages between firmwares. Needs to hold data while MCU is not unpowered */
SECTIONS
{
 .SHARED_RAM(NOLOAD) : {
 KEEP(*(.SHARED_RAM))
 } > SHARED_RAM
}
 
__sharedram_start__	= ORIGIN(SHARED_RAM);
__sharedram_size__	= LENGTH(SHARED_RAM);
__bootrom_start__	= ORIGIN(BOOT_FLASH);
__bootrom_size__	= LENGTH(BOOT_FLASH);
__slot1rom_start__	= ORIGIN(SLOT1_ROM);
__slot1rom_size__	= LENGTH(SLOT1_ROM);
__slot2rom_start__	= ORIGIN(SLOT2_ROM);
__slot2rom_size__	= LENGTH(SLOT2_ROM);
__clientrom_start__ = ORIGIN(CLIENT_ROM);
__clientrom_size__	= LENGTH(CLIENT_ROM);
 
/* offset to be used for locating the image header from start image address */
__fw_header_offset = 0x200;
 
/* offset to be used for locating firmware code (".text") after image header */
__fw_codestart_offset = 0x30;
 
/* bootloader configuration, stored at the last page of SHARED_CFG section */
__bootloader_cfg_addr = 0x080FF800;

Application's Flash linker scatter file:

INCLUDE memory_map.ld
 
/* Entry Point */
ENTRY(Reset_Handler)
 
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */
 
_Min_Heap_Size = 0x200 ; /* required amount of heap */
_Min_Stack_Size = 0x400 ; /* required amount of stack */
 
 
/* Sections */
SECTIONS
{
 /* The Vector table into SLOT1_ROM Rom type memory */
 .isr_vector : {
 . = ALIGN(4);
 KEEP(*(.isr_vector)) 	/* Startup code */
 . = ALIGN(4);
 } > SLOT1_ROM
 
 
 /* The application image header */
 .image_hdr : ALIGN(4) {
 	FILL(0xFF)
 	
 	. = ORIGIN(SLOT1_ROM) + __fw_header_offset;
	KEEP (*(.image_hdr))
 } > SLOT1_ROM
 
 
 /* The clientManiobra library image header */
 CLIENT_HDR : ALIGN(4) {
 	FILL(0xFF)
 	
 	. = __clientrom_start__;
 	KEEP (*(CLIENT_HDR))
 } > CLIENT_ROM
 
 
 /* The Client Library program code and other data into "CLIENT_ROM" slot in flash */
 .text2 :
 {
	FILL(0xFF)
	. = __clientrom_start__ + __fw_header_offset + __fw_codestart_offset;
	. = ALIGN(4);
	
	*clientManiobra.a:* (.text .text*) /* .text sections from Client Library (code) */
 } > CLIENT_ROM
 
 
 /* The program code and other data into "FLASH" Rom type memory */
 .text : {
 	FILL(0xFF)
 	. = ORIGIN(SLOT1_ROM) + __fw_header_offset + __fw_codestart_offset;
 . = ALIGN(4);
 		 										/* Before was: 		*(.text) 	*/
 		 										/* Before was: 		*(.text*) 	*/
 
 *(EXCLUDE_FILE (*clientManiobra.a) .text .text*)		/* .text sections (code) 		*/
 
 	*(.glue_7)
	*(.glue_7t)
 *(.eh_frame)									/* exception handling tables	*/
 
 KEEP (*(.init))
 KEEP (*(.fini))
 
 . = ALIGN(4);
 _etext = .; /* define a global symbols at end of code */
 } > SLOT1_ROM
 
... (continues)...

Withing "clientManiobra" library code, the following code snippets are implemented:

  • Structure definition:
typedef struct __attribute__((packed)) {
	uint32_t						magicWord;
	uint16_t 						imageFormatVersion;
	uint32_t 						crc;
	uint32_t 						data_size;
	uint8_t 						imageType;	
	uint16_t						clientFamily;
	uint8_t 						clientVersion;
	f_init_TypeDef 					func_init;		 /* callbacks */
	f_checkEndOfMsgCallback_TypeDef	func_EndOfMsgCbk;
	f_getCmdTypeDef					func_getCmd;
	f_getErrorTypeDef				func_getError;
	f_getRspTypeDef					func_getRsp;
	f_getUrcTypeDef					func_getUrc;
	f_extractElemTypeDef			func_extractElem;
	f_analyzeCmdTypeDef				func_analyzeCmd;
	f_analyzeParamTypeDef			func_analyzeParam;
	f_terminateCmdTypedef			func_terminateCmd;
	uint32_t 						reserved;	
} client_image_hdr_t;
  • In above structure definition every "func_xxxx" type is a function signature typedef. As example:
typedef void (*f_init_TypeDef)(uart_parser_context_t *p_upCtxt);
  • Code snippet creating the constant variable holding the structure content to be placed at the very beginning of "CLIENT_ROM" memory region:
/* Global variables of clientManiobra */
 
static const client_image_hdr_t client_hdr __attribute__((section("CLIENT_HDR"))) = {
		.magicWord			= CLIENT_IMAGE_MAGIC,
		.imageFormatVersion	= CLIENT_IMAGE_CURRENT_VERSION,
		.crc				= 0,				/* to be parsed in post-processing */
		.data_size			= 0x0000,	/* to be parsed in post-processing */
		.imageType			= IMAGE_TYPE_CLIENT_LIBRARY,
		.clientFamily		= CLIENT_FAMILY_ORONA_ARCA,
		.clientVersion		= CLIENT_ORONA_FW_VERSION,
		.func_init			= &libInit,
		.func_EndOfMsgCbk	= &lib_checkEndOfMsgCallback,
		.func_getCmd		= &lib_getCmd,
		.func_getError		= &lib_getError,
		.func_getRsp		= &lib_getRsp,
		.func_getUrc		= &lib_getUrc,
		.func_extractElem	= &lib_extractElem,
		.func_analyzeCmd	= &lib_analyzeCmd,
		.func_analyzeParam	= &lib_analyzeParam,
		.func_terminateCmd	= &lib_terminateCmd,
		.reserved			= 0
};

All compiles perfect but linking is raising error.

It's already 3 days reviewing where may I be mistaken but no progress. Any help/suggestion will be highly appreciated.

Pol

    This topic has been closed for replies.
    MM..1
    MM..1Best answer
    Super User
    March 20, 2022

    How big is your .a file?

    5 replies

    DBara.3
    DBara.3Author
    Associate
    March 20, 2022

    Sorry missed to add a snapshot in map generated file. Apparently linker is allocating every piece where it should but only weird thing is around the size of the "client_hdr" structure (equal to its position?)

    MM..1
    MM..1Best answer
    Super User
    March 20, 2022

    How big is your .a file?

    DBara.3
    DBara.3Author
    Associate
    March 20, 2022

    upps, 1.303KB !! :frowning_face_with_open_mouth:

    I was only focused on the header piece and didn't put attention on the overall library size...

    Thanks for your feedback !!! I need to focus on the library size it is amazing big and it shoudn't...

    Pol

    MM..1
    Super User
    March 20, 2022

    from screen part .text 0x37b3C (222k OK) , but part .text2 is chaos...

    DBara.3
    DBara.3Author
    Associate
    March 20, 2022

    I was able to fix clientManiobra.a size, now it is 45KB

    Nevertheless the error still is reproducing....

    make -j8 all 
    arm-none-eabi-gcc -o "Datalogger_DiscoL496_07.elf" @"objects.list" -mcpu=cortex-m4 -T"D:\LiftEye\devices\firmwares\ST\Datalogger_DiscoL496_07\STM32L496AGIX_FLASH.ld" --specs=nosys.specs -Wl,-Map="Datalogger_DiscoL496_07.map" -Wl,--gc-sections -static -L"D:\LiftEye\devices\firmwares\ST\Datalogger_DiscoL496_07" -L"D:\LiftEye\devices\firmwares\ST\libOronaArca\Debug" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
    c:\st\stm32cubeide_1.0.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: Datalogger_DiscoL496_07.elf section `CLIENT_HDR' will not fit in region `CLIENT_ROM'
    c:\st\stm32cubeide_1.0.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: region `CLIENT_ROM' overflowed by 269730352 bytes
    collect2.exe: error: ld returned 1 exit status
    make: *** [makefile:84: Datalogger_DiscoL496_07.elf] Error 1
    "make -j8 all" terminated with exit code 2. Build might be incomplete.
     
    18:44:50 Build Failed. 3 errors, 0 warnings. (took 2s.621ms)

    Having a look at generated .map file:

    .SHARED_RAM
     *(.SHARED_RAM)
     0x0000000020000000 __sharedram_start__ = ORIGIN (SHARED_RAM)
     0x0000000000000100 __sharedram_size__ = LENGTH (SHARED_RAM)
     0x0000000008000000 __bootrom_start__ = ORIGIN (BOOT_FLASH)
     0x0000000000008000 __bootrom_size__ = LENGTH (BOOT_FLASH)
     0x0000000008008000 __slot1rom_start__ = ORIGIN (SLOT1_ROM)
     0x000000000005a000 __slot1rom_size__ = LENGTH (SLOT1_ROM)
     0x0000000008062000 __slot2rom_start__ = ORIGIN (SLOT2_ROM)
     0x000000000005a000 __slot2rom_size__ = LENGTH (SLOT2_ROM)
     0x00000000080bc000 __clientrom_start__ = ORIGIN (CLIENT_ROM)
     0x000000000003c000 __clientrom_size__ = LENGTH (CLIENT_ROM)
     0x0000000000000200 __fw_header_offset = 0x200
     0x0000000000000030 __fw_codestart_offset = 0x30
     0x00000000080ff800 __bootloader_cfg_addr = 0x80ff800
     0x0000000020050000 _estack = (ORIGIN (RAM) + LENGTH (RAM))
     0x0000000000000200 _Min_Heap_Size = 0x200
     0x0000000000000400 _Min_Stack_Size = 0x400
     
    .isr_vector 0x0000000008008000 0x1ac
     0x0000000008008000 . = ALIGN (0x4)
     *(.isr_vector)
     .isr_vector 0x0000000008008000 0x1ac ./Core/Startup/startup_stm32l496agix.o
     0x0000000008008000 g_pfnVectors
     0x00000000080081ac . = ALIGN (0x4)
     
    .image_hdr 0x00000000080081ac 0x70
     FILL mask 0xff
     0x0000000008008200 . = (ORIGIN (SLOT1_ROM) + __fw_header_offset)
     *fill* 0x00000000080081ac 0x54 ff
     *(.image_hdr)
     .image_hdr 0x0000000008008200 0x1c ./App/Device_Core/app_device_logic.o
     
    CLIENT_HDR 0x00000000080bc000 0x80bc000
     FILL mask 0xff
     0x00000000080bc000 . = __clientrom_start__
     *fill* 0x00000000080bc000 0x80bc000 ff
     *(CLIENT_HDR)
     
    .text2 0x0000000010178000 0x80bc230
     FILL mask 0xff
     0x00000000080bc230 . = ((__clientrom_start__ + __fw_header_offset) + __fw_codestart_offset)
     *fill* 0x0000000010178000 0x80bc230 ff
     0x0000000018234230 . = ALIGN (0x4)
     *clientManiobra.a:*(.text .text*)
     
    .text 0x0000000008008220 0x37b3c
     FILL mask 0xff
     0x0000000008008230 . = ((ORIGIN (SLOT1_ROM) + __fw_header_offset) + __fw_codestart_offset)
     *fill* 0x0000000008008220 0x10 ff
     0x0000000008008230 . = ALIGN (0x4)
     *(EXCLUDE_FILE(*clientManiobra.a) .text .text*)
     .text 0x0000000008008230 0x40 c:/st/stm32cubeide_1.0.1/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/thumb/v7e-m+fp/hard/crtbegin.o
     .text.AT_init 0x0000000008008270 0x130 ./App/Cellular/Cellular_Core/AT_Core/at_core.o
     0x0000000008008270 AT_init
     .text.AT_open 0x00000000080083a0 0x210 ./App/Cellular/Cellular_Core/AT_Core/at_core.o
     0x00000000080083a0 AT_open
     .text.AT_open_channel
     0x00000000080085b0 0x1b4 ./App/Cellular/Cellular_Core/AT_Core/at_core.o
     0x00000000080085b0 AT_open_channel
     
    ... etc....

    In row 34, the provided size in the map file for section CLIENT_HDR is 0x80bc000 !!

    Any hints will be very much appreciated.