Skip to main content
LSant.6
Associate II
November 21, 2022
Question

I am looking for an easily available MCU to do a simple analog readout through a 32position mux and CAN-Bus connection. With my very limited understanding I looked at the stm32f0 series. But some of them are hard to find. Is there a better option? Th

  • November 21, 2022
  • 4 replies
  • 1143 views

..

    This topic has been closed for replies.

    4 replies

    LSant.6
    LSant.6Author
    Associate II
    November 21, 2022

    Is the stm32f072 a good solution for this? i have seen it to be available on jlc

    Tesla DeLorean
    Guru
    November 21, 2022

    ST has multiple part designations and pin configurations.

    There's certainly a subset of "STM32F072" that will support 1x CAN

    Expect to use a crystal or oscillator to meet CAN timing specifications, along with a suitable transceiver.

    Perhaps flesh out the rest of the design at a block/functional level.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    LSant.6
    LSant.6Author
    Associate II
    November 22, 2022

    Have looked at the STM32F072x8. It says on the datasheet that it has an internal crytal up to 32MHz. Do I need to add an external crystal or can it work with the internal one? This PCB will be conected to several clones and a "master"pcb which will send the collective information of all clones to an ecu. Can i also just place a good ecternal crystal on the "master"pcb and use the same clock over all boards? Sorry i have an unlimited ammount of questions...:)

    Andrei Chichak
    Lead
    November 21, 2022

    "easily available" isn't a thing currently. It's more like "get any dev board you can, figure out how to do what you need, find a processor that can be used".

    The distributors have about 1% of ST's processor list available. Mostly in ball grid, bluetooth, and multi-core. If you want something simpler, they're not "easily available".

    We've been told by our distributors to place orders for future delivery. If there are no orders, there is no production need, and no production.