Skip to main content
RSing.4
Associate
October 29, 2020
Question

I am interfacing Spi Flash AT25SF041 with STM32f030RC . while Debugging, i checked that SPI_I2S_FLAG is not able to SET.

 if ((SPIx->SR & SPI_I2S_FLAG) != (uint16_t)RESET)

 {

   /* SPI_I2S_FLAG is set */

   bitstatus = SET;

 }

 else

 {

   /* SPI_I2S_FLAG is reset */

   bitstatus = RESET;

 }

 /* Return the SPI_I2S_FLAG status */

 return bitstatus;

This topic has been closed for replies.

3 replies

TDK
October 29, 2020

I don't see a question here. What flag are you checking for?

"If you feel a post has answered your question, please click ""Accept as Solution""."
RSing.4
RSing.4Author
Associate
November 2, 2020

i am doing interfacing of external flash with stm32f030RC, when i am calling Erase function or write function, code is getting stuck in above loop.

waclawek.jan
Super User
November 2, 2020

Debugging may be intrusive. From RM:

Clearing the RXNE bit is performed by reading the SPIx_DR register.

JW