I am getting undefined reference to `HAL_WWDG_IRQHandler error even after defining #define HAL_WWDG_
I am working with a project which does not have .ioc file from STM32 cube mx, so I have to enable HAL functions and make these changes manually. I wanted to add a watchdog timer. Somehow the Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_wwdg.c file is not getting included in the build.
What I have done so far:
- Enabled wwdg module in conf file
- I have removed and included the HAL_Driver folder with HAL function includes and source in Include directories. Similary I have also done the same for folder with conf file.
Could anyone please guide me in understanding the issue?