Skip to main content
jendoubi saif ddine
Associate II
April 21, 2018
Question

html page with javascript can't be generated

  • April 21, 2018
  • 0 replies
  • 573 views
Posted on April 21, 2018 at 23:07

i have a html page that excute js functions so i add the needed file to fsdata.c but i can't manage to find the problem why it won't work 

  • fs_open(&file, '/pie.html');

    netconn_write(pAcceptedConnection, (const unsigned char*)(file.data), (size_t)file.len, NETCONN_NOCOPY);
  1. FsData.C

    #include 'lwip/apps/fs.h'

    #include 'lwip/def.h'

    #define file_NULL (struct fsdata_file *) NULL

    static const unsigned int dummy_align__samples_pie_html = 0;

    static const unsigned char data__samples_pie_html[] = {

    /* /samples/pie.html (18 chars) */

    0x2f,0x73,0x61,0x6d,0x70,0x6c,0x65,0x73,0x2f,0x70,0x69,0x65,0x2e,0x68,0x74,0x6d,

    0x6c,0x00,0x00,0x00,

    /* HTTP header */

    /* 'HTTP/1.0 200 OK

    ' (17 bytes) */

    ........ etc ...........

    0x0a,0x0a,0x0a,0x0a,0x0a,0x7d,0x29,0x2e,0x63,0x61,0x6c,0x6c,0x28,0x74,0x68,0x69,

    0x73,0x29,0x3b,0x0a,};

    const struct fsdata_file file__samples_pie_html[] = { {

    file_NULL,

    data__samples_pie_html,

    data__samples_pie_html + 20,

    sizeof(data__samples_pie_html) - 20,

    1,

    }};

    const struct fsdata_file file__404_html[] = { {

    file__samples_pie_html,

    data__404_html,

    data__404_html + 12,

    sizeof(data__404_html) - 12,

    1,

    }};

    const struct fsdata_file file__Chart_js[] = { {

    file__404_html,

    data__Chart_js,

    data__Chart_js + 12,

    sizeof(data__Chart_js) - 12,

    1,

    }};

    #define FS_ROOT file__Chart_js

    #define FS_NUMFILES 3
    This topic has been closed for replies.