Skip to main content
BDoon.1
Associate III
January 12, 2023
Solved

HSLV example code?

I am using a U585QI and have some external flash memory connected to an OCTOSPI. We are having some intermittent failures with it, and since we're powering the processor with 1.8v I want to try enabling HSLV for the Data/Clock lines. I found HAL_GPIO_EnableHighSPeedLowVoltage, but I'm not sure when to call it...

1) Is this a common use case for the high-speed-low-voltage functionality?

2) Is there any example code for this? Particularly the option bits aspect?

This topic has been closed for replies.
Mohamed Aymen HZAMI
ST Employee
January 18, 2023

Hello,

This is an example of OCTOSPI with HSLV configuration

/**
* @brief OSPI MSP Initialization
* This function configures the hardware resources used in this example
* @param hospi: OSPI handle pointer
* @retval None
*/
void HAL_OSPI_MspInit(OSPI_HandleTypeDef* hospi)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 if(hospi->Instance==OCTOSPI1)
 {
 /* USER CODE BEGIN OCTOSPI1_MspInit 0 */
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_CS_GPIO_PORT, OCTOSPI_CS_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_DQS0_GPIO_PORT, OCTOSPI_DQS0_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_DQS1_GPIO_PORT, OCTOSPI_DQS1_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_CLK_GPIO_PORT, OCTOSPI_CLK_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_NCLK_GPIO_PORT, OCTOSPI_NCLK_PIN);
 
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D0_GPIO_PORT, OCTOSPI_D0_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D1_GPIO_PORT, OCTOSPI_D1_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D2_GPIO_PORT, OCTOSPI_D2_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D3_GPIO_PORT, OCTOSPI_D3_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D4_GPIO_PORT, OCTOSPI_D4_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D5_GPIO_PORT, OCTOSPI_D5_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D6_GPIO_PORT, OCTOSPI_D6_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D7_GPIO_PORT, OCTOSPI_D7_PIN);
 
 /* USER CODE END OCTOSPI1_MspInit 0 */
 
 /** Initializes the peripherals clock
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_OSPI;
 PeriphClkInit.OspiClockSelection = RCC_OSPICLKSOURCE_SYSCLK;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* Peripheral clock enable */
 __HAL_RCC_OSPIM_CLK_ENABLE();
 __HAL_RCC_OSPI1_CLK_ENABLE();
 
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**OCTOSPI1 GPIO Configuration
 PC0 ------> OCTOSPIM_P1_IO7
 PC1 ------> OCTOSPIM_P1_IO4
 PC2 ------> OCTOSPIM_P1_IO5
 PA7 ------> OCTOSPIM_P1_IO2
 PC3 ------> OCTOSPIM_P1_IO6
 PB0 ------> OCTOSPIM_P1_IO1
 PB2 ------> OCTOSPIM_P1_DQS
 PA2 ------> OCTOSPIM_P1_NCS
 PA3 ------> OCTOSPIM_P1_CLK
 PA6 ------> OCTOSPIM_P1_IO3
 PB1 ------> OCTOSPIM_P1_IO0
 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF3_OCTOSPI1;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_6;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_2|GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 /* USER CODE BEGIN OCTOSPI1_MspInit 1 */
 
 /* USER CODE END OCTOSPI1_MspInit 1 */
 }
 
}

The High speed low voltage (HSLV) is a feature, when enabled it allow the GPIOs to reach higher frequencies. The only constraint is that Vdd must not exceed 2.5v (Vdd < 2.5v)

Mohamed Aymen

5 replies

Mohamed Aymen HZAMI
ST Employee
January 16, 2023

Hello @Community member​ and welcome to the community,

You need to enable HSLV of OCTOSPI pins before initializing its pins.

Mohamed Aymen

BDoon.1
BDoon.1Author
Associate III
January 16, 2023

@Mohamed Aymen HZAMI​ Does that mean calling HAL_GPIO_EnableHighSPeedLowVoltage before HAL_OSPI_Init? And does it mean I need to do it to run OSPI from a 1.8v VDD reliably?

Mohamed Aymen HZAMI
ST Employee
January 18, 2023

Hello,

This is an example of OCTOSPI with HSLV configuration

/**
* @brief OSPI MSP Initialization
* This function configures the hardware resources used in this example
* @param hospi: OSPI handle pointer
* @retval None
*/
void HAL_OSPI_MspInit(OSPI_HandleTypeDef* hospi)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 if(hospi->Instance==OCTOSPI1)
 {
 /* USER CODE BEGIN OCTOSPI1_MspInit 0 */
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_CS_GPIO_PORT, OCTOSPI_CS_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_DQS0_GPIO_PORT, OCTOSPI_DQS0_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_DQS1_GPIO_PORT, OCTOSPI_DQS1_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_CLK_GPIO_PORT, OCTOSPI_CLK_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_NCLK_GPIO_PORT, OCTOSPI_NCLK_PIN);
 
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D0_GPIO_PORT, OCTOSPI_D0_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D1_GPIO_PORT, OCTOSPI_D1_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D2_GPIO_PORT, OCTOSPI_D2_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D3_GPIO_PORT, OCTOSPI_D3_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D4_GPIO_PORT, OCTOSPI_D4_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D5_GPIO_PORT, OCTOSPI_D5_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D6_GPIO_PORT, OCTOSPI_D6_PIN);
 HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D7_GPIO_PORT, OCTOSPI_D7_PIN);
 
 /* USER CODE END OCTOSPI1_MspInit 0 */
 
 /** Initializes the peripherals clock
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_OSPI;
 PeriphClkInit.OspiClockSelection = RCC_OSPICLKSOURCE_SYSCLK;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* Peripheral clock enable */
 __HAL_RCC_OSPIM_CLK_ENABLE();
 __HAL_RCC_OSPI1_CLK_ENABLE();
 
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**OCTOSPI1 GPIO Configuration
 PC0 ------> OCTOSPIM_P1_IO7
 PC1 ------> OCTOSPIM_P1_IO4
 PC2 ------> OCTOSPIM_P1_IO5
 PA7 ------> OCTOSPIM_P1_IO2
 PC3 ------> OCTOSPIM_P1_IO6
 PB0 ------> OCTOSPIM_P1_IO1
 PB2 ------> OCTOSPIM_P1_DQS
 PA2 ------> OCTOSPIM_P1_NCS
 PA3 ------> OCTOSPIM_P1_CLK
 PA6 ------> OCTOSPIM_P1_IO3
 PB1 ------> OCTOSPIM_P1_IO0
 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF3_OCTOSPI1;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_6;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_2|GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 /* USER CODE BEGIN OCTOSPI1_MspInit 1 */
 
 /* USER CODE END OCTOSPI1_MspInit 1 */
 }
 
}

The High speed low voltage (HSLV) is a feature, when enabled it allow the GPIOs to reach higher frequencies. The only constraint is that Vdd must not exceed 2.5v (Vdd < 2.5v)

Mohamed Aymen

BDoon.1
BDoon.1Author
Associate III
January 18, 2023

Awesome, thank you! Can you confirm that this is something I should be doing to get reliable OSPI communication when powered at 1.8v?

Mohamed Aymen HZAMI
ST Employee
January 30, 2023

Hello @Community member​,

If you are targeting higher frequencies at Vdd < 2.5V, yes it is recommended to Enable the HSLV.

Mohamed Aymen