Skip to main content
David Ashman
Associate II
January 18, 2022
Question

HSE oscillator when using USB

  • January 18, 2022
  • 1 reply
  • 777 views

The STM32F303xB datasheet states that HSE oscillator should be used when using USB. I suspect it is because of the degraded accuracy of the HSI oscillator at temperature. I've had issues with CAN not working well with HSI at elevated temperature. Does anyone have experience using HSI vs. HSE for USB-CDC class virtual COM port? Thanks!

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
January 19, 2022

I don't think there is much experience out there. Why would anybody want to have an unreliable element in an already wacky interface, which has the potential to bite you in the least convenient moment?

Try to have a look at the HSI using oscilloscope.

Some STM32 out there can condition an internal RC oscillator based on USB SOF, but not the 'F3.

JW