Associate II
Mar 26, 2017 11:42 PM UTC
Solved
HSE Bypass Clock Source w/CubeMX and Nucleo 303ZE fails
- 2 replies
- 914 views
Posted on March 27, 2017 at 01:42
Possible bug in CubeMX 4.20.0?
Using Nucleo 303ZE board, and Atollic 7.1.1
Build dead simple default project, except in RCC, set High Speed Clock to 'BYPASS Clock Source', and select HSE as input to PLL.
In main.c you'll have this routine:
void SystemClock_Config(void)
{RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL2; RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); },,, etc,
Results in bad return from HAL_RCC_OscConfig() and call to Error_Handler().
If you change this line:
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;
to
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
it runs fine.
Not sure if there is something I don't understand, or if it is possibly a bug in CubeMX. my .ioc file attached.