Skip to main content
Associate II
November 9, 2024
Question

HRTIM Alternate function output open drain mode not supported

....so says STM32F334x4/x6/x8 Errata sheet STM32F334x4/x6/x8 Rev Z device limitations

Doc is dated 2021. No answers seen on web.

Has this been fixed yet?

If not, will it be fixed? And if so, when?

Ta lots

Rex

 

 

 

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
November 11, 2024

Hello @RexG 

unfortunately, there is not any available workaround for now and there is not any potential solution on going. For the typo on table 4 where it is mentioned that there is an existing workaround. It is just a typo on the errata sheet that I've escalated for correction on the coming release (under internal ticket number 196061).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RexGAuthor
Associate II
November 12, 2024

That's a very simple mask fix!

Badly done ST!