Question
How works the function HAL_SAI_Transmit_DMA()
Posted on July 26, 2017 at 09:58
Hi Communities,
can any body please explain me, how works exactly the function HAL_SAI_Transmit_DMA(). I am using STM32F746VGTX.
This is one example:
uint8_t TestArray[4] = {0x00,0xff,0x00,0x00};
HAL_SAI_Transmit_DMA(hsai, TestArray, 1);
my configuration of Sai for the transmitter:
hsai_BlockA1.Instance = SAI1_Block_A;
hsai_BlockA1.Init.AudioMode = SAI_MODEMASTER_TX;hsai_BlockA1.Init.Synchro = SAI_ASYNCHRONOUS;hsai_BlockA1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;hsai_BlockA1.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE;hsai_BlockA1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_FULL;hsai_BlockA1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_8K;hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;hsai_BlockA1.Init.MonoStereoMode = SAI_STEREOMODE;hsai_BlockA1.Init.CompandingMode = SAI_NOCOMPANDING;hsai_BlockA1.Init.TriState = SAI_OUTPUT_NOTRELEASED;if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_PCM_LONG, SAI_PROTOCOL_DATASIZE_16BIT, 2) != HAL_OK){Thank you for your help!
#sai-hal_sai_transmit_dma