Skip to main content
Apill
Associate III
Oct 8, 2018 9:09 PM UTC
Solved

How/ Where can i download stm32 cube mx version 4.21?

I am working with SD card in SDIO mode. The current version of cube mx i.e, 4.27 is not working. Some people in the community posted that after version 4.21 SD card issue is persistent. so i would like to download 4.22

Youtube link I have followed:

https://www.youtube.com/watch?v=Y5UMTGQDmog&t=523s

hardware used:

https://www.amazon.com/Mciro-Memory-Shield-Module-Board/dp/B0797LG1CY/ref=asc_df_B0797LG1CY/?tag=hyprod-20&linkCode=df0&hvadid=241935719665&hvpos=1o2&hvnetw=g&hvrand=11359505135560567974&hvpone=&hvptwo=&hvqmt=&hvdev=c&hvdvcmdl=&hvlocint=&hvlocphy=9013830&hvtargid=pla-422072932282&psc=1

kit: Discovery f429.

https://www.amazon.com/32F429IDISCOVERY-STM32F429I-DISCO-Discovery-STM32F429ZIT6-Development/dp/B01EJ3GEJO

Basic code :

FATFS myFATFS;

FIL myFILE;

UINT testByte;

if(f_mount(&myFATFS,SDPath,1)==FR_OK)

{

HAL_GPIO_TogglePin(GPIOG,GPIO_PIN_14);

char myPath [] = "WRITE1.TXT\0";

f_open(&myFILE, myPath, FA_WRITE | FA_CREATE_ALWAYS);

char myData[]= "Hello World\0";

f_write(&myFILE, myData, sizeof(myData), &testByte);

f_close(&myFILE);

HAL_Delay(1000);

HAL_GPIO_TogglePin(GPIOG, GPIO_PIN_13);

}

    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Oct 8, 2018 11:04 PM UTC

    https://community.st.com/s/question/0D50X00009XkYVDSA3/please-provide-a-way-to-download-older-version-of-the-cube

    SDIO interface clashes with LCD on STM32F429-DISCO, the original STM32F4-DISCO is a different board.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    1 reply

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Oct 8, 2018 11:04 PM UTC

    https://community.st.com/s/question/0D50X00009XkYVDSA3/please-provide-a-way-to-download-older-version-of-the-cube

    SDIO interface clashes with LCD on STM32F429-DISCO, the original STM32F4-DISCO is a different board.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..