Skip to main content
VChau
Associate II
May 16, 2022
Question

How Watch Dog Timer works in STOP mode? STOP mode time is more than 5 min. I want to implement WDT in STOP mode but STOP mode time is more than 5 min and WDT reset time is less than 30 sec.

..

This topic has been closed for replies.

4 replies

KnarfB
Super User
May 16, 2022

The RTC can be used for wake up after an arbitrarily long time.

hth

KnarfB

VChau
VChauAuthor
Associate II
May 18, 2022

Agree, I'm using RTC to Wake up

My question is

What happen if device Hang up (not work properly) in real time scenario(In real application)? How could I reset if device goes Hang up(halt fault)

VChau
VChauAuthor
Associate II
May 16, 2022

Thanks for writing, but currently I'm using RTC for wake up....do some take and go back to sleep....

but some time firmware get hang up or stuck some where, So I want to use WDT but i don't know "how

WDT works in Sleep mode"

KnarfB
Super User
May 16, 2022

The IWDG can continue counting while the MCU is in low power modes or it can pause counting then. So you may set your RTC to wake up say every 4 minutes and the IWDG to 5 minutes. The RTC can then reset the IWDG. What kind of errors do you want the WDG to care for while the MCU is in STOP mode?

hth

KnarfB