Skip to main content
duongtomho
Associate
January 18, 2019
Solved

How to wake-up on time in time with RTC ?

Hi eveyone,

I have a problem with RTC wake up. I use LSE 32.768kHz.

I run example from manufacturer to wake up MCU from Stand by mode very 1min, 2mins. Everything work okay.

But, When I put delay 10s and HAL_PWR_EnterSTANDBYMode(); into while(1). Everything is not okay.

The RTC does not wake up on time, when I delay 10s it will lack of 10s, when I delay 20s it lack of 20s. I try to do it many times.

How can I wake-up mcu on time in time I set?

Thank you for any help.

int main(void)
{
 HAL_Init();
 
 /* Configure LED3 */
 BSP_LED_Init(LED3);
 
 /* Configure the system clock to 2 MHz */
 SystemClock_Config();
 
 /* Configure the system power */
 SystemPower_Config();
 
 /* Check and handle if the system was resumed from StandBy mode */ 
 if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
 {
 /* Clear Standby flag */
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); 
 }
 
 /* Disable Wakeup Counter */
 HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle);
 
 /*## Setting the Wake up time ############################################*/
 /* RTC Wakeup Interrupt Generation:
 Wakeup Time Base = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSE or LSI))
 Wakeup Time = Wakeup Time Base * WakeUpCounter 
 = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSE or LSI)) * WakeUpCounter
 ==> WakeUpCounter = Wakeup Time / Wakeup Time Base
 
 To configure the wake up timer to 4s the WakeUpCounter is set to 0x1FFF:
 RTC_WAKEUPCLOCK_RTCCLK_DIV = RTCCLK_Div16 = 16 
 Wakeup Time Base = 16 /(~39.000KHz) = ~0,410 ms
 Wakeup Time = ~4s = 0,410ms * WakeUpCounter
 ==> WakeUpCounter = ~4s/0,410ms = 9750 = 0x2616 */
 HAL_RTCEx_SetWakeUpTimer_IT(&RTCHandle, 0x2616, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
 
 /* Insert 5 seconds delay */
 HAL_Delay(5000);
 
 /* Clear all related wakeup flags */
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
 
 
 
 while (1)
 {
	HAL_Delay(10000);
 
	/* Request to enter STANDBY mode (Wake Up flag is cleared in PWR_EnterSTANDBYMode function) */
	HAL_PWR_EnterSTANDBYMode();
 }
}

This topic has been closed for replies.
Mohamed Aymen HZAMI
ST Employee
January 24, 2019

Hello,

Why you do not set the wake up time by setting the wake counter in the HAL_RTCEx_SetWakeUpTimer_IT function.

Instead of adding the "HAL_Delay" function, you can simply customize your wake up time like this:

- For example if you want to waking-up the MCU after 10 seconds:

  • Wakeup Time Base = 16 (RTC Clock Div) /(39.000KHz) = 0,410 ms
  • Wakeup Time = 10s = 0,410ms * WakeUpCounter
    • WakeUpCounter = 10s /0,410ms = 24 390= 0x5F46

You need just to calculate the value that you want to set.

Best Regards,

Mohamed Aymen.

5 replies

Mohamed Aymen HZAMI
ST Employee
January 22, 2019

Hello,

I think that you are working with an STM32L4 device ?

Why you put the HAL_PWR_EnterSTANDBYMode() in the while(1) loop ?

Best Regards,

Mohamed Aymen.

duongtomho
Associate
January 23, 2019

Hello mohamed-aymen.hzami,

I use STM32L151

I put HAL_PWR_EnterSTANDBYMode(), because I want to run my program in while(1). After that I put microcontroller into stanby mode, and it will wake up after 1min

I try to use HAL_RTC_DeInit(&hrtc); after call HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, timeMin, RTC_WAKEUPCLOCK_CK_SPRE_16BITS); and before call  HAL_PWR_EnterSTANDBYMode(), I call HAL_RTC_DeInit(&hrtc);

My program run and wake up on time. But In the first run, it wake-up immediately, after that it run true. I don't know why.

Below its my code. Thanks for your attention.

int main(void)
{
 HAL_Init();
 
 /* Configure LED3 */
 BSP_LED_Init(LED3);
 
 /* Configure the system clock to 2 MHz */
 SystemClock_Config();
 
 /* Configure the system power */
 SystemPower_Config();
 
 /* Check and handle if the system was resumed from StandBy mode */ 
 if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
 {
 /* Clear Standby flag */
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); 
 }
 
 /* Disable Wakeup Counter */
 HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle);
 
 /*## Setting the Wake up time ############################################*/
 /* RTC Wakeup Interrupt Generation:
 Wakeup Time Base = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSE or LSI))
 Wakeup Time = Wakeup Time Base * WakeUpCounter 
 = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSE or LSI)) * WakeUpCounter
 ==> WakeUpCounter = Wakeup Time / Wakeup Time Base
 
 To configure the wake up timer to 4s the WakeUpCounter is set to 0x1FFF:
 RTC_WAKEUPCLOCK_RTCCLK_DIV = RTCCLK_Div16 = 16 
 Wakeup Time Base = 16 /(~39.000KHz) = ~0,410 ms
 Wakeup Time = ~4s = 0,410ms * WakeUpCounter
 ==> WakeUpCounter = ~4s/0,410ms = 9750 = 0x2616 */
 HAL_RTCEx_SetWakeUpTimer_IT(&RTCHandle, 0x2616, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
 
 /* Insert 5 seconds delay */
 HAL_Delay(5000);
 
 /* Clear all related wakeup flags */
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
 
HAL_RTC_DeInit(&hrtc);
 
 
 while (1)
 {
	HAL_Delay(10000);
 
	/* Request to enter STANDBY mode (Wake Up flag is cleared in PWR_EnterSTANDBYMode function) */
 HAL_RTC_Init(&hrtc);
 
	HAL_PWR_EnterSTANDBYMode();
 }
}

Mohamed Aymen HZAMI
ST Employee
January 24, 2019

Hello,

Why you do not set the wake up time by setting the wake counter in the HAL_RTCEx_SetWakeUpTimer_IT function.

Instead of adding the "HAL_Delay" function, you can simply customize your wake up time like this:

- For example if you want to waking-up the MCU after 10 seconds:

  • Wakeup Time Base = 16 (RTC Clock Div) /(39.000KHz) = 0,410 ms
  • Wakeup Time = 10s = 0,410ms * WakeUpCounter
    • WakeUpCounter = 10s /0,410ms = 24 390= 0x5F46

You need just to calculate the value that you want to set.

Best Regards,

Mohamed Aymen.

HDaji.1
Senior
February 21, 2024

@Mohamed Aymen HZAMI 

If I want MCU to go to standby/stop mode for 10 hours, the counter value should be

  • WakeUpCounter = 36000s/0.41s = 87804.

However, it does not work. In my test, MCU wakes up just a few seconds nor matter how big WakeUpCounter is assigned.

Pkemarco
Associate II
April 10, 2024

Hello @HDaji.1 

For the WakeUpCounter you have to take into account the counter deepth and the clock.

If you use RTC_WAKEUPCLOCK_RTCCLK_DIV2 as the clock, then you'll just have 2^16 * (2/32000) ≈ 4s, 32000 here is my origine clock (32K LSI), si it can change according to your situation.

But if you use RTC_WAKEUPCLOCK_CK_SPRE_16BITS (1Hz clock), then you can last 2^16 / (1Hz * 3600s) ≈  18.2 hours.

And if you want to go even further, you can use RTC_WAKEUPCLOCK_CK_SPRE_17BITS (0.5Hz), and you will be able to last 2^16 / (0.5Hz * 3600s)  ≈ 36.4 Hours.

So, if you want to stop for 10 hours, you can use :

 

HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 36000, RTC_WAKEUPCLOCK_CK_SPRE_16BITS, 36000);