How to use X-CUBE-AVS 1.0.1 for 32F746GDISCOVERY (STM32F746NG MCU), which is has hex file for 32F769IDISCOVERY ?
I have 32F746GDISCOVERY (STM32F746NG MCU) board and wanted to use Amazon voice service on it. But the X-CUBE-AVS 1.0.1 program present on STM website is for 32F769IDISCOVERY board. Also it contains the binaries and hex file for 32F769IDISCOVERY. I tried to compile the project using IAR Embedded workbench for 32F746GDISCOVERY as target controller but the .out file i get after this can not be loaded on 32F746GDISCOVERY. Also i tried to load the existing hex file of 32F769IDISCOVERY on 32F746GDISCOVERY , but failed.
I don't know much about embedded programming, so i was wondering if i have to convert the project or the output file from 769 to 746 to work.
Please share your feedback if someone has already tried and knows the solution..
Attaching the hex file of 769. Also present on STM web site.
Thanks in advance
#stm32f746ngh6 #32f746gdiscovery-3d-model-solid #32f746gdiscovery #32f769idiscovery #avs #stm32f746ng #x-cube-avs