Skip to main content
Associate III
April 12, 2024
Solved

How to use SPI in other .c

Hi everybody,

 

Actually I start a new project with a ST7567 driver for LCD 128x64.

 

I have create my project with CubeIDE . CubeIDE generate my code in the main.c  like this :

 

 

 

 

/* Private variables ---------------------------------------------------------*/
RTC_HandleTypeDef hrtc;

SPI_HandleTypeDef hspi1;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_RTC_Init(void);
static void MX_SPI1_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

 

 

 

 

 

It's ok .

 

Now to drive my screen I would like to create files like st7567_driver.h and a st7567_driver.c file.

This way I could create my functions relating to the driver in these files. Functions such as "draw pixel", "send command", "send data", etc....

But to communicate with the driver I have to use SPI1 create in my main.c.

So I get an error when I try to use the HAL_SPI_Transmit function in st7567_driver.c

I don't know how to declare to my st7567_driver.c file as I use the SPI1 declare in my main.c

Thank you for your help

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
April 12, 2024

You need to add 

extern SPI_HandleTypeDef hspi1;

in st7567_driver.c

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

10 replies

Associate III
April 12, 2024

"So I get an error when I try to use the HAL_SPI_Transmit function in st7567_driver.c"

Can you show us the error ?

JJoao.1Author
Associate III
April 12, 2024

of course,

 

My code in the st7567_driver.c :

#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include <errno.h>

#include "st7567_driver.h"

void st7567_write_cmd(uint8_t cmd)
{
	HAL_GPIO_WritePin(A0_GPIO_Port, A0_Pin, 0);
	HAL_SPI_Transmit(&hspi1, cmd, 1, 10);
}

and the error

../Core/Src/st7567_driver.c: In function 'st7567_write_cmd':
../Core/Src/st7567_driver.c:39:27: error: 'hspi1' undeclared (first use in this function)
 39 | HAL_SPI_Transmit(&hspi1, cmd, 1, 10);
 | ^~~~~
../Core/Src/st7567_driver.c:39:27: note: each undeclared identifier is reported only once for each function it appears in
../Core/Src/st7567_driver.c:39:34: warning: passing argument 2 of 'HAL_SPI_Transmit' makes pointer from integer without a cast [-Wint-conversion]
 39 | HAL_SPI_Transmit(&hspi1, cmd, 1, 10);

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
April 12, 2024

You need to add 

extern SPI_HandleTypeDef hspi1;

in st7567_driver.c

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
April 12, 2024

Hello,

You need to provide details about the error.

Meanwhile, did you include stm32l0xx_hal.h in st7567_driver.h or st7567_driver.c?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
April 12, 2024

@JJoao.1 wrote:

I don't know how to declare to my st7567_driver.c file as I use the SPI1 declare in my main.c

Thank you for your help


This is standard C programming stuff - nothing specifically to do with STM32.

Detailed example in this post:

https://community.st.com/t5/stm32cubeide-mcus/adding-new-c-source-files-to-my-project-and-navigating-through/m-p/657455/highlight/true#M25847

and note this follow-up:

https://community.st.com/t5/stm32cubeide-mcus/adding-new-c-source-files-to-my-project-and-navigating-through/m-p/658310/highlight/true#M25925

 


@JJoao.1 wrote:

I get an error


As the others have said, we need to know what error you get (and where) in order to help you to solve that error!

If it's a build error, copy & paste the full text of the message from the 'Console' window; post it as for source code.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
April 12, 2024

 And maybe cast the second parameters of HAL_SPI_Transmit to (uint8_t *), or change the prototype of

void st7567_write_cmd(uint8_t cmd)

to

void st7567_write_cmd(uint8_t *cmd)

 

JJoao.1Author
Associate III
April 12, 2024

Okay thank you so much. That works !

which is the best solution of the two cast

solution1

void st7567_write_cmd(uint8_t cmd)
{
	HAL_GPIO_WritePin(A0_GPIO_Port, A0_Pin, 0);
	HAL_SPI_Transmit(&hspi1, (uint8_t*)&cmd, 1, 10);
}

 

Or solution 2

void st7567_write_cmd(uint8_t * cmd)
{
	HAL_GPIO_WritePin(A0_GPIO_Port, A0_Pin, 0);
	HAL_SPI_Transmit(&hspi1, cmd, 1, 10);
}

 Maybe it's similar ?

Andrew Neil
Super User
April 12, 2024

@JJoao.1 wrote:

 Maybe it's similar ?


yes - they both achieve the same end.

The question is really which one is most convenient for you to use in your application. Only you can answer that.

 

EDIT

There's really no need for the cast here:

 

void st7567_write_cmd(uint8_t cmd)
{
	HAL_GPIO_WritePin(A0_GPIO_Port, A0_Pin, 0);
	HAL_SPI_Transmit(&hspi1, (uint8_t*)&cmd, 1, 10);
}

 

cmd is defined as a uint8_t, therefore &cmd will naturally give a uint8_t* result - no need to cast it.

In fact, I might venture to say that it's best not to cast it - as that could hide future errors; eg, if you later changed the definition of cmd to a uint16_t...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
April 12, 2024

I would say that two is more readable, make more sense

JJoao.1Author
Associate III
April 12, 2024

Thank you so much for your reactivity. I can continue my learning and my code

 

Best regards