Skip to main content
Arman Ilmak
Senior
November 17, 2021
Question

How to use NAND flash ECC

  • November 17, 2021
  • 0 replies
  • 1143 views

Hi everyone

Im still dealing with nand flash and im at the ecc part now :).

I found a very good topic in ST but i still had questions and that topic was closed.

https://community.st.com/s/question/0D50X00009XkZjD/nand-flash-fsmc-and-ecc?t=1637138511900

There is a register that defines the ecc_page_size.

Tesla said that for 256 bytes ECC generates 3 bytes ECC.

When we config ecc_page_size to 2048 still ECC generate 3 bytes for these or it generates 24 bytes and gives us a pointer to read that (i think its not true because i didnt see any pointers in stm32 cube generated code).

The second question is that after write page we have to get_ecc from hardware to store in spare area and after read we have to get_ecc from hardware and read last ecc from spare to compare these two or not?

The last question is that how can i correct the data if error was detected?

This topic has been closed for replies.