how to use just Rx pin of an uart
Hi, I have a sensor that send data over uart to a stm32f722 uC. This sensor is powered at the same time of uC.
I've noticed that some times the sensor stop sending data. For example, if the code is running ok and then reboot the uC some times the sensor stop working. UART is configured as Transmitter and receiver, so I think that during initialization Tx pin from uC is sending some garbage and so the sensor stop working (the sensor is waiting for a 'space' char on Rx pin to stop and show a menu to the user configuration). So I would like to leave the Tx pin of the uC without use. How can i do that? I can configure Receiver only on cubeide, but it config the Tx pin anyway.
Is there a way to leave Tx pin of uart5 as reset state while Rx pin of uart5 is working?
Thank