Skip to main content
HReis.1
Associate
March 27, 2022
Question

How to use i2c extension connector on stm32f769i-discovery

UM2033 mentions that Wi-fi connector of stm32f769i-discovery development board can be configured for i2c board using signals EXT_SCL and EXT_SDA that are connected to PG3 and PG6, however datasheet of MCU (DS11532) these pins do not support I2C.

Is this configuration intended for a software solution?

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
March 27, 2022

It looks like you'd do this as bit-bang I2C,along with changing the solder bridges.

Not sure there are any examples where this is used.

If you need I2C perhaps use the D14/D15 on the Arduino connection PB9/PB8

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate
September 14, 2024

Hello Tesla:

          Since PB8 and PB9 have been used for other purposes, I can only use PG3 and PG6,the extension I2C connector.After I change the port to PG3 and PG6,how can I configure the port, but the interface will become low, so that it is always busy and cannot be used? I really need your help.Thanks.