Skip to main content
po221
Senior
August 8, 2022
Solved

How to trim the STM32 HSI easily

  • August 8, 2022
  • 11 replies
  • 4057 views

Hello

I'm using a stm32L431 with an STLinkV3

https://www.st.com/en/microcontrollers-microprocessors/stm32l4x1.html#documentation

HSI is enabled at 16MHz for USART2, used to receive a 1200Bd signal.

I receive wrong characters because of the trim.

I understood the principle of trim and its registers, in particular thanks to this doc

dm00425536-how-to-optimize-stm32-mcus-internal-rc-oscillator-accuracy-stmicroelectronics-2.pdf

My question: is there a way to adjust this trim automatically via cubeIDE and stlinkV3?

Maybe another solution less practical but more practical than a manual adjustment?

Thanks in advance

This topic has been closed for replies.
Best answer by po221

It's definitely not a TRIM problem, I was able to reproduce the problem with a usb converter that knows how to transfer data as well.

I opened another topic: parity problem

https://community.st.com/s/question/0D53W00001ixfc7SAA/usart2-on-stm32l431-does-not-support-parity-with-cubemx

Thank you very much for your help and clarification.

11 replies

gbm
Super User
August 8, 2022

It used to be a well known problem with HAL and it probably still is. The HAL overwrites the calibration values for internal clock sources, actually de-calibrating them. So, either do not use HAL, or add two lines of code to main() function - save the RCC->ICSCR to some variable before the clock config call and put the stored value back to RCC->ICSCR after the call.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
po221
po221Author
Senior
August 8, 2022

Hello

Thank you for your reply

Do I understand that without HAL the trim is calibrated by default at the time of programming? (by the STlinkV3??)

For the moment I change the trim value manually via cubeMx, so via the HAL layer precisely

gbm
Super User
August 8, 2022

Wrong. The callibration value is written to system ROM once by ST during tests. It's transferred to the trim register during uC bootup, then overwritten by HAL firmware for no reason.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
S.Ma
Principal
August 8, 2022

Use debug mode, and before running the code, check the hw trim register values. After code runs for few seconds, stop the code and check again. If the values have chemged...

Remember that trim is only a first order tuning. HSI will drift in temperature and maybe voltage. The higher the baudrate the more precise the clock must be.

gbm
Super User
August 8, 2022

Wrong again. Clock accuracy should be no worse than 2% regardless of the baud rate. This assumes that the other communicating party also has 2% clock tolerance. Relative error should not exceed 4%.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Tesla DeLorean
Guru
August 8, 2022

Isn't it one of these things that's depend on temperature and voltage? If I were designing this I'd have a bunch of coefficients, but alas...

Many of the STM32 have a TIM which can measure HSI vs HSE/PLL, I guess "easy" would be to feed a solid 10 MHz in via HSE_IN, or timestamp a 32-bit TIM vs external 1PPS

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
po221
po221Author
Senior
August 8, 2022

by "easy" I mean, calibrated automatically by an autocalibration (an other source) or by the stlinkV3 pod.

My previous microcontrollers from another manufacturer were calibrated when downloading a program in the flash, by the pod.

I realize that the accuracy of HSI (at worst +/- 4%) should not give me any worries

I am modifying the trim and I cannot correct my problem... some characters are well received, others are crazy.

Tesla DeLorean
Guru
August 8, 2022

Well 1200 baud's certainly not something with ppm/ppb expectations. The STM32 method for dividing down, and granularity of the BRR, tends to work against higher frequencies. For lower frequencies you can also tune via the BRR, in APB clock units.

If you're fixturing during programming, or have something else that's crystal derived, and you can generate for the test, or related to equipment you normally attach too, you could always do some time domain measurements of the serial signal, as a reference.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal
August 8, 2022

Newer parts have usart with autobaud featurr which is problably used in some bootloaders. An easier solution than trimming.

po221
po221Author
Senior
August 8, 2022

L431 has autobaud rate functionality on USART2 !

I'm not sure I understand ABRMOD and ABREN. Is the correction done automatically permanently by the usart?

Thanks

po221
po221AuthorBest answer
Senior
August 9, 2022

It's definitely not a TRIM problem, I was able to reproduce the problem with a usb converter that knows how to transfer data as well.

I opened another topic: parity problem

https://community.st.com/s/question/0D53W00001ixfc7SAA/usart2-on-stm32l431-does-not-support-parity-with-cubemx

Thank you very much for your help and clarification.