How to STOP USART during hitting breakpoint in debug on STM32G071
I have 3 USARTs working on my STM32G071 nucleo board. One is for communication with PC and transfering settings registers. Second one comunicate with GPS. And third one just resend everything received from GPS module, it enables me see in PC, what GPS sending to MCU. When I need to debug code, I put breakpoint into place, where I have to examine code and when MCU hits breakpoint, it stops. But GPS still transmitting data and controller (should be paused on breakpoint) still retransmitting data to USART3. This is not behavior, which I need. I need to stop everything in controller, when code hist breakpoint. Is it possible to do that? I use LL libraries.