Skip to main content
Hardeep Singh
Associate II
November 20, 2019
Question

How to stabilize the SDADC2 in STM32F373VCT6?

  • November 20, 2019
  • 0 replies
  • 445 views

When I connect a voltage source to channel 0 of SDADC2 in single ended mode, then at floating pin and connecting to ground the value displayed is full scale which 65535, while when I connect some voltage like 2V or 3V to same channel then it shows the result fixed as 32738. I checked the software configuration refereing to the Reference Manual and have connected VREF to 3.3V which is VDD.

This topic has been closed for replies.