Skip to main content
CDew.1
Associate III
May 17, 2024
Solved

How to sleep when USB_VBUS on stm32f105 is low?

I have a self-powered device.  It appears as a USB CDC device /dev/ttyACM0, when plugged into a Linux host.  The device port is wired to USB_VBUS, so that pin will only be high when connected to a USB host.

I would like to detect the presence of the USB cable, so that the device can sleep if there is no cable and other conditions are met.

- How can I detect the presence of the USB cable?  I'm using CubeIDE and the HAL.

- How can I put the STM32 to sleep in such a way that it will wake up when the USB cable is plugged back in?

 

This topic has been closed for replies.
CDew.1
CDew.1Best answer
Associate III
May 20, 2024

I've found a solution:

int usb_plugged_in = HAL_GPIO_ReadPin(PMU_LED_PWR_GPIO_Port, PMU_LED_PWR_Pin / 2);

where PMU_LED_PWR is the name of PA10.  PA9 is on the same port as PA10 and its pin mask is right-shifted.

 

i.e. Setting PA9 to the role of USB_OTG_FS_VBUS makes it a GPIO input at a lower level, but doesn't give you a name to reference it.  By calculating USB_OTG_FS_VBUS's port struct and pin mask, you can access it.

 

4 replies

ST Technical Moderator
May 20, 2024

Hi @CDew.1 

If your device is self-powered, you can configure a GPIO pin to detect the VBUS level. 

Generally, to wake up a FS device from a suspend state, the host needs to drive low D+ to the K-State. Check section 28.5.2 Peripheral states in Reference Manual

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
CDew.1
CDew.1Author
Associate III
May 20, 2024

Thanks for your reply.  My self-powered device is always USB device and never a host.

I currently have PA9 configured as USB_OTG_FS_VBUS.

- Will USB (device) continue to work if I change PA9 to a GPIO_Input?

- Or do I need to rework the board to route VBUS to an *additional* GPIO pin?

(I was hoping that there was a HAL_ function which I could poll to see if USB_OTG_FS_VBUS was high.)

CDew.1
CDew.1AuthorBest answer
Associate III
May 20, 2024

I've found a solution:

int usb_plugged_in = HAL_GPIO_ReadPin(PMU_LED_PWR_GPIO_Port, PMU_LED_PWR_Pin / 2);

where PMU_LED_PWR is the name of PA10.  PA9 is on the same port as PA10 and its pin mask is right-shifted.

 

i.e. Setting PA9 to the role of USB_OTG_FS_VBUS makes it a GPIO input at a lower level, but doesn't give you a name to reference it.  By calculating USB_OTG_FS_VBUS's port struct and pin mask, you can access it.