How to set up the adc sampling time.
Hi,
I am using ADC of STM32H743ZI which is configured as 16 bit, ADC clock =36.5MHz,Tsampling=1.5cycles in continuous conversion mode . I am using DMA technique to collect the data using a buffer size of 4096 in circular mode.
The input is sine wave of peak to peak voltage =3.3V whose frequency varies from 1Hz to 20K Hz.
In debug mode when I observed data stored in buffer I am able reconstruct the signal back but accuracy is very less (sample to sample there is lot of voltage difference) for high frequencies.
Since Tsampling is 1.5cycles and Tconversion is 8.5Cycles and ADC clock is 36.5 MHz sampling speed would be 3.65Msamples/sec.
What might be the issue for this low accuracy whether DMA is not able to store this high sampling speed data or Tsamping is creating a problem. Can any one help me out solving this problem.