Skip to main content
sam239955
Associate III
December 6, 2011
Question

How to set up MDK-ARM, cmsis, stlib 3.5.0 for 16Mhz HSE

  • December 6, 2011
  • 1 reply
  • 439 views
Posted on December 07, 2011 at 00:25

Hi,

i want to know how to setup my stm32f103ze (HD) project correctly to 16mhz HSE. I build up a device with 16mhz NOT 8mhz. I want to use USB and USART too.

It would be nice to have a helping hand.

with regards

sam

    This topic has been closed for replies.

    1 reply

    sam239955
    sam239955Author
    Associate III
    December 7, 2011
    Posted on December 07, 2011 at 01:52

    the solution:

    USE_STDPERIPH_DRIVER, STM32F10X_HD, HSE_VALUE=16000000

    in keil as preprocessor variable

    and set XTAL to 16.0

    here is my init of rcc_clocks for my stm32f103zet6

    /******************************************************************************/

    /* SETUP.C: Setup Functions                                                     */

    /* IMU200 16MHz HSE      72Mhz = 16Mhz/2*9                                    */

    /******************************************************************************/

    #include ''stm32f10x.h''                            /* STM32F10x Library Definitions      */

    #include ''misc.h''

    #include ''Setup.h''

    extern volatile unsigned char  Clock1s;

    extern volatile unsigned char  Clock100ms;

    extern volatile unsigned long  TimeTick;

    /* Variables */        

    ErrorStatus HSEStartUpStatus;

    GPIO_InitTypeDef  GPIO_InitStructure;

    I2C_InitTypeDef  I2C_InitStructure;

    SPI_InitTypeDef  SPI_InitStructure;

    USART_InitTypeDef USART_InitStructure;

    void SetupClock (void)

    {

     /* SYSCLK, HCLK, PCLK2 and PCLK1 configuration -----------------------------*/   

         

      /* RCC system reset(for debug purpose) */

      RCC_DeInit();

      /* Enable HSE */

      RCC_HSEConfig(RCC_HSE_ON);

      /* Wait till HSE is ready */

      HSEStartUpStatus = RCC_WaitForHSEStartUp();

      if(HSEStartUpStatus == SUCCESS)

      {

        /* Enable Prefetch Buffer */

        FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);

        /* Flash 2 wait state */

        FLASH_SetLatency(FLASH_Latency_2);

     

        /* HCLK = SYSCLK */

        RCC_HCLKConfig(RCC_SYSCLK_Div1);

     

        /* PCLK2 = HCLK */

        RCC_PCLK2Config(RCC_HCLK_Div1);

        /* PCLK1 = HCLK/2 */

        RCC_PCLK1Config(RCC_HCLK_Div2);

        /* On STICE the PLL output clock is fixed to 72 MHz */

        RCC_PLLConfig(RCC_PLLSource_HSE_Div2, RCC_PLLMul_9);

        /* Enable PLL */

        RCC_PLLCmd(ENABLE);

        /* Wait till PLL is ready */

        while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET)

        {

        }

        /* Select PLL as system clock source */

        RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);

        /* Wait till PLL is used as system clock source */

        while(RCC_GetSYSCLKSource() != 0x08)

        {

        }

     }

    /* set SysTick */

        SysTick_Config(72*1000*10);

    /* Enable GPIO Clocks */

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD, ENABLE);

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOE, ENABLE);

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOF, ENABLE);

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);    

    }