Skip to main content
eittinfo
Associate II
February 25, 2017
Question

How to set stm32f407 sdio to 48Mhz?

  • February 25, 2017
  • 3 replies
  • 1094 views
Posted on February 25, 2017 at 17:25

hi 

i want use sdio as 8bit mode and 48Mhz but i try to do this and i saw max 25Mhz on clk line for sdio port.

how can i set sdio as 8bit-48Mhz mode?

tnx for replay

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    February 25, 2017
    Posted on February 25, 2017 at 17:36

    You'd need to use BYPASS mode to get the Q tap clock (48 MHz nominally) as the bus clock. If you use the divider the minimum setting will be DIV2

    There are timing issues with the BYPASS mode (see errata), but the SDIO clock can be up to 75 MHz, assuming you don't need it for USB, or CRYPT/HASH, which would give you 37.5 MHz safely.

    Bandwidth on the SDIO is more critically limited by transfer size, small block reads/writes have significant overhead.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    eittinfo
    eittinfoAuthor
    Associate II
    February 25, 2017
    Posted on February 25, 2017 at 18:07

    tnx for your replay.

    i use this code to config sdio clock

    SDIO->CLKCR  = /*SDIO_CLKCR_HWFC_EN |*/ (SDIO_CLKCR_WIDBUS_0*2) | SDIO_CLKCR_PWRSAV | SDIO_CLKCR_CLKEN | (1);

    i use logic analyzer to capture clk speed,with this config ,clk was around 16.6 mhz ,and if i set (0) for divide value i got around 24Mhz clk speed.

    how can i disable divider?

    i use usb host in my project.

    Tesla DeLorean
    Guru
    February 25, 2017
    Posted on February 25, 2017 at 18:32

    >>

    how can i disable divider?

    Like I said, you'd need to use the BYPASS mode.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..