Skip to main content
waclawek.jan
Super User
August 24, 2019
Question

How to set RTC_PRER in STM32F0xx?

  • August 24, 2019
  • 0 replies
  • 473 views

RM0091 rev.9 in 25.7.5 RTC prescaler register (RTC_PRER) says:

The initialization must be performed in two separate write accesses. Refer to Calendar initialization and configuration on page 584.

However, Calendar initialization and configuration does not say, what two separate write accesses; regarding RTC_PRER it only says:

3. To generate a 1 Hz clock for the calendar counter, program both the prescaler factors in

RTC_PRER register.

I see more than that e.g. in RM0090 (i.e. the 'F4xx RM), but does that apply to to 'F0?

Or is the two writes not necessary for the more modern 'F0, and the remark at the register description is just a copy/paste artifact?

Could this please be properly documented?

Thanks,

JW

This topic has been closed for replies.