Skip to main content
Asantos
Associate III
Jun 16, 2020 9:16 PM UTC
Question

How to set H7 ADC to synchronous clock mode??

..

This topic has been closed for replies.

2 replies

TDK
Jun 17, 2020 1:44 AM UTC

Can you describe what you're looking to do in more detail? You cannot sample multiple channels simultaneously with the same ADC.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Asantos
AsantosAuthor
Associate III
Jun 17, 2020 2:14 PM UTC

Hi,

Synchronous clock mode is when ADC clock is derived from the system clock (AHB clock). STM32CubeMX don't allows to select Synchronous clock mode, I want to know why?

I tried to configure ADC at register level with:

using H7 rev V.

AHB clock = 200MHZ

CKMODE = 0x02

ADC_CLK_INPUT = HCLK/2 = 100MHZ, rev V divide the clock by 2, => Fadc_ker_ck = 50MHZ.

With this configuration, the ADC2 fails to calibrate.

If I do:

ADC clock from PLL2P = 200MHZ

ADC12_COMMON->CCR.CKMODE = 0x00; (asynchronous clock mode)

ADC12_COMMON->CCR.PRESC = 1; (PLL2P/2 = 100MHZ)

ADC2 calibrate and works correctly for the same clock input.

I'm trying to configure the ADC to Synchronous clock mode using the STM32CubeMX to compare the generated code with my register level configuration code.