Skip to main content
Associate III
Mar 24, 2025 4:39 AM UTC
Solved

How to set a memory address to GPDMA_CxLBAR register when only 16 bit region is open to hold the address?

My linked-list object's base address in memory is 0x200bffbc.   How can I save this address in GPDMA_CxLBAR register (that holds "the linked-list base address of the memory region, for a given channel x, from which the LLIs describing the programmed sequence of the GPDMA transfers, are conditionally and automatically updated")  when GPDMA_CxLBAR designated region for the address (LBA[31:16]) is only 16 bits long?

 

Anyone can help please? 

This topic has been closed for replies.
psabelaBest answer
Associate III
Apr 20, 2025 7:41 AM UTC

Example of creating link list in code
and setting GPDMA_CxLBAR and GPDMA_CxLLR registers.

//Create GPDMA link list in code. Example:
//1. Link list item:
typedef struct {
 volatile uint32_t CTR1_register; 
 volatile uint32_t CTR2_register; 
 volatile uint32_t CBR1_register; 
 volatile uint32_t CSAR_register; //Source address for the transfer.
 volatile uint32_t CDAR_register; //Destination address for the transfer.
 volatile uint32_t CTR3_register;
 volatile uint32_t CBR2_register;
 volatile uint32_t CLLR_register; 
} LinkListItem_t;

//2. List object with 2 linked list items and their memory address:
typedef struct {
 LinkListItem_t node1; //node1 address: 0x200bffa8 (same as base address)
 LinkListItem_t node2; //node2 address: 0x200bffc8
} LinkList_t; //base address: 0x200bffa8


GPDMA channel x linked-list base address register (GPDMA_CxLBAR):
In this example, the address of the link list structure object is 0x200bffa8

GPDMA_CxLBAR->LBA = 0x200b
GPDMA_CxLBAR = 0x200b0000



GPDMA channel x linked-list address register (GPDMA_CxLLR):

The address of node1 is 0x200bffa8.  Node 0 (staring value of LLR) points to node 1.
f      |f      |a      |8
1111|1111|1010|1000
11|1111|1110|1010|00
    Bits LA[15:2]Bits 1:0 Reserved
3  |f      |e      |a

//Bits 15:2 LA[15:2]: pointer (16-bit low-significant address) to the next linked-list data structure
pNode0->CLLR_register.LA = 0x3fea;
pNode0->CLLR_register = 0xfe01ffa8; //the last 4 hex values aggree to the last 4 hex of the address 


The address of node2 is 0x200bffc8.  The node 1 points to node 2.
f      |f      |c      |8   
1111|1111|1100|1000
11|1111|1111|0010|00  Bits LA[15:2]Bits 1:0 Reserved
3 |f       |f      |2

//Bits 15:2 LA[15:2]: pointer (16-bit low-significant address) to the next linked-list data structure
pNode1->CLLR_register.LA = 0x3ff2;
pNode1->CLLR_register = 0xfe01ffc8; //the last 4 hex values aggree to the last 4 hex of the address 

The node 2 points back to node 1. (The address of node1 is 0x200bffa8.)

//Bits 15:2 LA[15:2]: pointer (16-bit low-significant address) to the next linked-list data structure
pNode2->CLLR_register.LA = 0x3fea;
pNode2->CLLR_register = 0xfe01ffa8; //the last 4 hex values aggree to the last 4 hex of the address 




cc @Amel NASRI 

 

 

 

 

 

3 replies

psabelaAuthor
Associate III
Apr 1, 2025 1:54 AM UTC

Never mind.  Got it at last.

Amel NASRI
ST Technical Moderator
Apr 3, 2025 1:34 PM UTC

Hi @psabela ,

Glad to know that your issue is resolved.

But how you did? That may be interesting for other to know and avoid facing a similar problem.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
psabelaAuthorBest answer
Associate III
Apr 20, 2025 7:41 AM UTC

Example of creating link list in code
and setting GPDMA_CxLBAR and GPDMA_CxLLR registers.

//Create GPDMA link list in code. Example:
//1. Link list item:
typedef struct {
 volatile uint32_t CTR1_register; 
 volatile uint32_t CTR2_register; 
 volatile uint32_t CBR1_register; 
 volatile uint32_t CSAR_register; //Source address for the transfer.
 volatile uint32_t CDAR_register; //Destination address for the transfer.
 volatile uint32_t CTR3_register;
 volatile uint32_t CBR2_register;
 volatile uint32_t CLLR_register; 
} LinkListItem_t;

//2. List object with 2 linked list items and their memory address:
typedef struct {
 LinkListItem_t node1; //node1 address: 0x200bffa8 (same as base address)
 LinkListItem_t node2; //node2 address: 0x200bffc8
} LinkList_t; //base address: 0x200bffa8


GPDMA channel x linked-list base address register (GPDMA_CxLBAR):
In this example, the address of the link list structure object is 0x200bffa8

GPDMA_CxLBAR->LBA = 0x200b
GPDMA_CxLBAR = 0x200b0000



GPDMA channel x linked-list address register (GPDMA_CxLLR):

The address of node1 is 0x200bffa8.  Node 0 (staring value of LLR) points to node 1.
f      |f      |a      |8
1111|1111|1010|1000
11|1111|1110|1010|00
    Bits LA[15:2]Bits 1:0 Reserved
3  |f      |e      |a

//Bits 15:2 LA[15:2]: pointer (16-bit low-significant address) to the next linked-list data structure
pNode0->CLLR_register.LA = 0x3fea;
pNode0->CLLR_register = 0xfe01ffa8; //the last 4 hex values aggree to the last 4 hex of the address 


The address of node2 is 0x200bffc8.  The node 1 points to node 2.
f      |f      |c      |8   
1111|1111|1100|1000
11|1111|1111|0010|00  Bits LA[15:2]Bits 1:0 Reserved
3 |f       |f      |2

//Bits 15:2 LA[15:2]: pointer (16-bit low-significant address) to the next linked-list data structure
pNode1->CLLR_register.LA = 0x3ff2;
pNode1->CLLR_register = 0xfe01ffc8; //the last 4 hex values aggree to the last 4 hex of the address 

The node 2 points back to node 1. (The address of node1 is 0x200bffa8.)

//Bits 15:2 LA[15:2]: pointer (16-bit low-significant address) to the next linked-list data structure
pNode2->CLLR_register.LA = 0x3fea;
pNode2->CLLR_register = 0xfe01ffa8; //the last 4 hex values aggree to the last 4 hex of the address 




cc @Amel NASRI