Skip to main content
MKado.1
Associate
April 7, 2022
Question

How to Send And Recive CAN Data in STM32F105 ?

  • April 7, 2022
  • 3 replies
  • 1174 views

i do that in STM Discovery 407 and it is work but the same in stm32f105 do not work ?

This topic has been closed for replies.

3 replies

ST Technical Moderator
April 7, 2022

Hello @MKado.1​ and welcome to the Community :)

Please share more details about your issue, so that it will be easier to understand the issue.

When debugging, are there any error ?

Did you checked the CAN examples available in the Cube packages?

Make sure that you configure correctly the CAN (pins, rate, clock, ...)

I advise your to review the CAN example available under STM32CubeF1 MCU package:

STM32Cube_FW_F1_Vx.x.x\Projects\STM3210E_EVAL\Examples\CAN\CAN_Networking

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MKado.1
MKado.1Author
Associate
April 7, 2022

this is my sending function there in no error

void CAN1_TX(uint32_t id,uint32_t dlc,uint8_t frame[8])

{

  CAN_TxHeaderTypeDef TxHeader;

  uint32_t TxMailbox;

  TxHeader.DLC = dlc;

  TxHeader.StdId = id;

  TxHeader.IDE = CAN_ID_STD;

  TxHeader.RTR = CAN_RTR_DATA;

  if(HAL_CAN_AddTxMessage(&hcan1, &TxHeader, frame,&TxMailbox) != HAL_OK){

    Error_Handler();

  }

  while(HAL_CAN_IsTxMessagePending(&hcan1, TxMailbox));

}

this is the settings image and the colck is ok 8mhz ext and working on 72mhz

0693W00000LxCpXQAV.pngMX_CAN1_Init();

 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_SET);

 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_15, GPIO_PIN_SET);

 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_14, GPIO_PIN_SET);

 //set filter / mask to accept every identifier

 CAN_FilterTypeDef filter = {0};

 filter.FilterIdHigh = 0x0000;

 filter.FilterIdLow = 0x0000;

 filter.FilterMaskIdHigh = 0;

 filter.FilterMaskIdLow = 0;

 filter.FilterFIFOAssignment = CAN_RX_FIFO0;

 filter.FilterBank = 0;

 filter.FilterMode = CAN_FILTERMODE_IDMASK;

 filter.FilterScale = CAN_FILTERSCALE_16BIT;

 filter.FilterActivation = ENABLE;

 filter.SlaveStartFilterBank = 0;

 if (HAL_CAN_ConfigFilter(&hcan1, &filter) != HAL_OK)

   return (1);

 HAL_CAN_Start(&hcan1);

i set the filter also and not reciving any thing .. but let me solve the sending befor

and this is the loop for sending and there is a flashin led as you see

if (tm>1000)

{

 HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_15);

 CAN1_TX(0x321,8,Von_260_1);

 tm=0;

}

the program is workinh good and flashing the led and go in the function CAN1_TX and do not sending any thing

there is a NUVOTON board connecting to my STM board to recive

and i made tha same thing in STM Discovery working good ... but in STM 105 not working

i do not know what you need to know also ??

thank you for response and i am waiting for the answer :)

MKado.1
MKado.1Author
Associate
April 7, 2022

and there is a logic analyzer connected to the CAN Bas to see the Data but there is no data of course

anf the NUVOTON board sending its data as an ACK for STM board Data