Skip to main content
CDew.1
Associate III
Mar 23, 2020 4:06 PM UTC
Solved

How to send a single USART character under interrupt, on an STM32H743?

I have the following code, which is *almost* always working. (It typically gets stuck after 10-100K characters.)

void USART3_IRQHandler(void)
{
	if (LL_USART_IsActiveFlag_TXE(USART3)) {
		stats.txe++;
		if (LL_USART_IsEnabledIT_TXE(USART3)) {
			LL_USART_EnableIT_TC(USART3);
			LL_USART_DisableIT_TXE(USART3);
		}
	}
	if (LL_USART_IsActiveFlag_TC(USART3)) {
		stats.tc++;
		if (txbusy) {
			txbusy = 0;
		} else {
			Error_Handler();
		}
		LL_USART_DisableIT_TC(USART3);
	}
}

The intent is that txbusy should be set false once the serial port is ready to accept another outgoing character. (The type of txbusy is a global "volatile _Bool".)

The code above works for 10-100K characters, but then an interrupt is missed, txbusy is left as 1 and the rest of the program stalls.

What is the reliable way of sending single characters, and being able to test (without blocking) whether another character can be sent without corrupting the last character? (I want to poll to see if another character can be safely sent, in an infinite loop containing other tasks. No RTOS is in use.)

(I initially tried just using TXE, but I found I was missing ~30% of characters. The combined TXE/TC code does not miss characters, but does eventually gets stuck.)

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
Mar 23, 2020 4:17 PM UTC

> The type of txbusy is a global "volatile _Bool"

But, how is txbusy used? If you are polling txbusy, why are you using the interrupt and not polling the flag(s) instead?

10 replies

KnarfB
KnarfBBest answer
Super User
Mar 23, 2020 4:17 PM UTC

> The type of txbusy is a global "volatile _Bool"

But, how is txbusy used? If you are polling txbusy, why are you using the interrupt and not polling the flag(s) instead?

CDew.1
CDew.1Author
Associate III
Mar 23, 2020 4:21 PM UTC

You can poll to see if it is safe to write a character? Could you point me at documentation? (I'm new to the STM32.)

KnarfB
Super User
Mar 23, 2020 4:43 PM UTC

RM0433 Reference manual Chapter 48.

Tesla DeLorean
Guru
Mar 23, 2020 4:32 PM UTC

Seems convoluted , can't you just service the TXE with data from a buffer?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
CDew.1
CDew.1Author
Associate III
Mar 24, 2020 9:18 AM UTC

No, sorry, I have been instructed to do this character by character. It's not about efficiency, it's about working with (and not changing) existing code.

KnarfB
Super User
Mar 23, 2020 4:33 PM UTC
 while( (USART1->ISR & USART_ISR_TXE) == 0 );
 USART1->TDR = ... // next char

I don't use H7 but should work the same. There maybe LL macros for it too.