Skip to main content
Associate III
May 23, 2025 2:51 PM UTC
Question

How to sample improve ADC speed?

My application senario: sample the sensor signal every second, and transmit through UART. 

to save power supply, I select ADC single mode, and used average as filter.

void ConfigureADC(void)
{
ADC1->CFGR1 |= ADC_CFGR1_AUTOFF;
ADC1->CFGR2 = (ADC1->CFGR2 & (~ADC_CFGR2_CKMODE))
| (ADC_CFGR2_OVSE | ADC_CFGR2_OVSR_2 | ADC_CFGR2_OVSR_1 | ADC_CFGR2_OVSR_0| ADC_CFGR2_OVSS_2); 
ADC1->SMPR |= ADC_SMPR_SMP_0 | ADC_SMPR_SMP_1 | ADC_SMPR_SMP_2; 
ADC1->CR |= ADC_CR_ADEN; 
ADC->CCR |= ADC_CCR_VREFEN|ADC_CCR_TSEN; 
}


unsigned int SignleADC(unsigned long int channel)
{
ADC1->CHSELR = channel; 
ADC1->CR |= ADC_CR_ADSTART;
while ((ADC1->ISR & ADC_ISR_EOC) == 0) 
{
}
ADC1->CR |= ADC_CR_ADSTP;
return ADC1->DR;
}

unsigned int Sensor_Read(void)
{
unsigned int gas[128];
unsigned long int read=0;
for(unsigned char i=0;i<128;i++)
gas[i] = SignleADC(ADC_CHSELR_CHSEL5);
for(unsigned char i=0;i<128;i++)
read += gas[i];

read = read>>7;
return((unsigned int)read);
}

Now the run time for Sensor_Read is about 700ms, it's too long, how can I improve the speed?

 

This topic has been closed for replies.

8 replies

Tesla DeLorean
Guru
May 23, 2025 2:58 PM UTC

The most obvious would be to sum/average over fewer samples, or use the longer sample/hold to negate the need.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
STM32L09Author
Associate III
May 23, 2025 3:11 PM UTC

thanks, but 128 is minimum, otherwise the noise too high

TDK
May 23, 2025 3:17 PM UTC

Convert with DMA in background. Perform averaging on demand when you send out sample.

"If you feel a post has answered your question, please click ""Accept as Solution""."
mƎALLEm
ST Technical Moderator
May 23, 2025 3:22 PM UTC

Hello @STM32L09 ,

In next time please use </> button to paste your code. See this post. I've edited your post.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
STM32L09Author
Associate III
May 24, 2025 12:53 AM UTC

got it.

STM32L09Author
Associate III
May 24, 2025 1:47 PM UTC

currently my idea is:

1. Configure ADC and DMA to sample PA0 and PA5 16 times

2. Re-configure ADC and DMA to sample PA5 256-16 times

repeat step 1.