Skip to main content
baswaraj
Associate
November 12, 2009
Question

how to run ucos on stm32

  • November 12, 2009
  • 6 replies
  • 2500 views
Posted on November 12, 2009 at 14:56

how to run ucos on stm32

    This topic has been closed for replies.

    6 replies

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:29

    Hi,

    I suggest you to purchase the Micrium's newest RTOS µC-OS/III bundle: a two-part book accompanied by an ST STM32F107 evaluation board.

    1) The 1st part covers the internals of µC/OS-III

    2) The 2nd part provides specific examples for using µC/OS-III on the

    popular STM32

    Available At

    http://www.amazon.com/Performance-Preemptive-Multitasking-Microprocessors-Microcontrollers/dp/0982337531/ref=sr_1_4?ie=UTF8&s=books&qid=1252537882&sr=1-4

    This is a good starting point and you will have a new board :)

    Cheers,

    STOne-32.

    [ This message was edited by: STOne-32 on 11-11-2009 20:35 ]

    baswaraj
    baswarajAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:29

    Hi,

    I am working on STM32F103RET6. I am new to ucos. could anyone tell me the steps to run ucos on stm32. I got the source code from Micrium for Keil. So i need to know how to run and where to see the result.

    goway_xu
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:29

    I ports ucos-ii 2.86 for STM32F103VCT6 with MDK4.01.

    You can check out the code with SVN:

    http://cortexm3.googlecode.com/svn/trunk

    The project path:

    cortexm3\ST\Project\uCOS-II-Manley

    It's run ok, and use 3.1.2 libs.

    baswaraj
    baswarajAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:29

    actually we have developed our own stm32f103ret6/bt6 boards interfacing with usb, mmc, gsm, gps, rfid, uart, lcd and i2c. With the help of st site we have written many applications without RTOS, now we are trying to write Applications in Ucos, thats the reason requesting you to help us.

    Regards,

    Baswaraj K

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:29

    Have you read the book mentioned by STOne-32 earlier...?

    baswaraj
    baswarajAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:29

    Hi,

    Im even trying to port uclinux on stm32f103ret6 (64 pin), i have studied the document from

    http://www.st.com/stonline/products/literature/an/16051.htm

    Im little bit confused from where i have to start like how to port uclinux on to stm32f103ret6 (64 pin) where i dont have any external NOR flash, but i have SD card interface with my board.could you please help me out in this.

    Mean while im going through the links which you have sent to me.

    Regards,

    Baswaraj K