Skip to main content
luisfynn1
Associate II
Dec 10, 2025 7:51 AM UTC
Question

how to run QSPI ?

Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code and a linker script content. Please read this post: How to insert source code.

Hi everyone,

I'm trying to interface an ICNA3306 LCD display using STM32's QSPI peripheral. The LCD uses a custom protocol where commands are sent as:

  • Instruction: 0x02 (8 bits, 1-wire)
  • Address: 0x00, CMD, 0x00 (24 bits, 1-wire)

Expected behavior: 32 clock pulses (8 instruction + 24 address) Actual behavior: Only 8 clock pulses (instruction only - address phase not transmitted)

Here's my code:

HAL_StatusTypeDef ICNA3306_WriteCommand(uint8_t cmd)
{
QSPI_CommandTypeDef sCommand = {0};

sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction = 0x02;

sCommand.AddressMode = QSPI_ADDRESS_1_LINE;
sCommand.AddressSize = QSPI_ADDRESS_24_BITS;
sCommand.Address = (0x00 << 16) | (cmd << ‌‌ | 0x00;

sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
sCommand.DataMode = QSPI_DATA_NONE;
sCommand.DummyCycles = 0;
sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;
sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;

return HAL_QSPI_Command(&hqspi, &sCommand, HAL_MAX_DELAY);
}

 

QSPI Configuration:

hqspi.Init.ClockPrescaler = 13;
hqspi.Init.FifoThreshold = 4;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_HALFCYCLE;
hqspi.Init.FlashSize = 23;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_6_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;

 

Oscilloscope shows:

luisfynn1_0-1765352949409.png

 

and then right waveform is below:(make QSPI using GPIO)

luisfynn1_1-1765352987189.png

 

3 replies

mƎALLEm
ST Technical Moderator
Dec 10, 2025 8:20 AM UTC

Hello,

I don't see any relation between the title and the request. Could you please clarify?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
luisfynn1
luisfynn1Author
Associate II
Dec 10, 2025 1:48 PM UTC

oh I am sorry.

I fixed it.

mƎALLEm
ST Technical Moderator
Dec 10, 2025 1:57 PM UTC

You need also to provide the MCU product part number you are using.

How to write your question to maximize your chances to find a solution

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.